This test compares the digital modulation power level to the CW power level at the same frequency. The external I/Q inputs are driven by a signal generator. A power meter and power sensor are used to measure the DUT output power in CW mode and in digital-modulation mode. The difference between the two power levels is compared to the specifications.
|
Test Equipment |
Recommended Models |
Alternate Models |
|
External Baseband |
N5182B Opt 656 or 657 |
N5182A Opt 651, or 652, or 654 |
|
Power Meter |
N1914A3 |
E4419A/B |
|
Power Sensor |
E9304A |
E9304A Opt H18 |
|
||
|
|
|
This test uses flexible power sensor channel assignment and will identify the channel that a power sensor is connected to using the ability of "smart" sensors such as the N848xA, U848xA, and E930xA series to report their full model and serial number.
Select from the links below for connection setups depending on the power sensor.
If this performance test fails, perform the following steps in order:
Check the equipment setup (see above). If the setup is incorrect, make the necessary corrections and rerun the performance test.
Refer to the troubleshooting section of the service guide. If you do not have a printed copy of the service guide (Option OBW), one is available either on the CD-ROM that came with your signal generator shipment or search for your signal generator model number on the Keysight website.
If necessary, obtain service from Keysight Technologies. Refer to Contacting Keysight Technologies.