This section lists the test equipment needed to run performance tests, adjustments, any critical specification requirements, and recommended model numbers. The required options will vary depending on the test to be performed. The computer and all test equipment are connected to the device under test (DUT) using GPIB.
|
|
In all test equipment configurations, cables and adapters must be properly torqued. Exceeding recommended torque values can cause damage to a cable or adapter, and can cause inaccurate test results. |
|
|
|
There are two equipment list tables on this page:
|
Test Equipment |
Recommended Model(s) |
Alternate Model(s) |
Applicable Tests/Comments |
|
Analyzers |
|||
|
Spectrum Analyzer
|
N9030B Opt 5xx1, MPB2, Pxx3, and N9063EM0E Analog Demodulation Measurement application4, 5
|
N9030A Opt 5xx1, MPB2, Pxx3, and N9063EM0D Analog Demodulation Measurement application4, 5, 6 E444xA7, 8 Options: [1109 or 1DS9], 12310, 23311, 24112, 23A13, B7J14 Click here for option footnotes.
|
AM Frequency Response (Internal) Inertial Landing System (Localized) Inertial Landing System (Glide Slope) |
|
Vector Signal Analyzer1
|
89441A Options AYA, AYH, AY9, B7A, and UFG or UTH |
|
|
|
Vector Signal Analysis Application1 N5162A, N5182A, N5172B, N5182B DUT only
|
89600 VSA with these options:
NOTES:
|
|
|
|
Measuring Receiver1
|
8902A |
|
|
|
Audio Analyzer1
|
8903B |
|
|
|
Sources |
|||
|
External Baseband N5162A, N5182A, N5172B, N5182B DUT only |
N5182B Opt 656 or 657 |
N5182A Opt 651, or 652, or 654 E4438C Opt 001 or 002 or 601 or 602, and Opt 4001 E4430B Opt UN8 & Opt 2002
|
|
|
Signal Generator |
N5182B Options 506, 1EA, and FRQ |
|
Required for the N5182BX07. |
|
Function Generator |
33622A |
33611A |
|
|
Reference Source For N5181B, N5182B, N5182N only |
E8257D Opt UNT, UNY, and 1EU
|
E8267D Opt UNT, UNY |
|
|
Meters and Sensors |
|||
|
Power Meter |
N1914A1, 2
|
E4419A/B |
|
|
Power Sensor (See below for calibration service ordering guidelines.) |
E9304A
E9304A Opt H19
|
E9304A H181
|
Digital Modulation Power Level Accuracy Relative to CW
|
|
Digital Multimeter |
3458A Opt 002 |
34470A |
|
|
Oscilloscopes |
|||
|
High Frequency Oscilloscope Mainframe |
N1000A |
86100A/B/C/D |
|
|
Oscilloscope Plug-in |
N1045B
|
N1045A1, 2
|
|
|
Local Oscillator1 For these DUTs only: N5162A, N5182A, N5172B, N5182B, N5182N
|
E8257D Opt [UNR or UNX or UNY] |
E8241A Opt UNJ
|
|
|
Attenuators |
|||
|
20 dB Attenuator |
8493A Opt 020 |
8490D Opt 020 |
|
|
10 dB Attenuator |
8491A Opt 010 |
8490D Opt 010 |
|
|
Other Devices |
|||
|
Frequency Counter |
53230A Opt 106 or 115 |
53132A Opt 050 or 124
|
|
|
20 GHz Mixer1 For these DUTs only: N5162A, N5182A, N5172B, N5182B, N5182N
|
0955-2225 |
0955-1017 |
|
|
Phase Noise System |
N5511A Options 504, CH21
|
E5505A |
|
To use the PXA N9030A with N9063EM0E analog demodulation measurement application functionality above 3.5 GHz, the N9030A must be upgraded with one of the following upgrade options: MTU or TES. After either upgrade, the N9030A must be re-calibrated for analog demodulation specifications above 3.5 GHz to be valid.
Choose from one of the following options:
Option MTU — Multi-Touch User Interface
For analog demodulation specifications above 3.5 GHz to be valid, Option MTU can only be installed on N9030A instruments with serial number prefix greater than or equal to MY/SG/US5449.
Option TES — TOI Enhanced Specifications
Option TES is a Keysight-only internal option. Keysight service centers need to contact the CSG support node to obtain an internal license key for this option.
USB power sensors require a power meter with USB ports. The table below shows the various options that will provide USB ports on the TME recommended N1914A power meter.
|
Test Equipment |
Recommended Model(s) |
Alternate Model(s) |
Applicable Tests/Comments |
|
Spectrum Analyzer
|
PXA N9030B Options MPB1, Pxx2
|
PXA N9030A Options MPB1, Pxx2
PSA models Options 1231, [1DS or 110]2:
|
ALC Calibration
|
|
Network Analyzer |
N5247B Options [423 or 425], 080, and 088
|
N5245B1 Options [423 or 425], 080, and 088 N5247A/AS2 Options 420, 423, 080, and 088 N5245A/AS2 Options 420, 423, 080, and 088 |
Required for N5182BX07 Frequency Extender Flatness/Atten Calibration adjustment. |
|
Signal Generator |
N5182B Options 506, 1EA, and FRQ |
|
Required for the N5182BX07. |
|
Power Sensor (See below for calibration service ordering guidelines.) |
E9304A Opt H19 |
|
|
|
E9304A E9304A Opt H18 |
N8482A1,2
|
||
|
Power Meter |
N1914A1
|
E4419A/B |
|
|
Cal Kit, ECal, Type-N |
N4690D-M0F |
N4690B-M0F |
|
|
Cable, 2.4 mm (f) to 2.4 mm (m)
|
8121-2065 |
|
|
|
Adapter, 2.4 mm (f) to Type-N (m) |
11903D |
|
|
|
Adapter, 2.4 mm (f) to Type-N (f) |
11903B |
|
Use the following guidelines to ensure power sensors used by N78xxA applications receive the correct calibration service:
Order Option 1A7 when ordering new power sensors that will be used as working standards in N7800A TME calibrations.
When ordering periodic calibration for instruments used as lab standards in the N7800A software, we recommend using “Keysight Cal + Uncertainties + Guardbanding”. More information can be found at http://www.keysight.com/find/americas_cal.
The N7800A software incorporates the ISO GUM Uncertainty in point-to-point uncertainty calculations. The special “H-series” calibration options (shown on the Special Calibrations Matrix located at http://cal.software.keysight.com) provide lower measurement uncertainties through use of direct comparison to devices directly characterized by NPL or NIST (or another NMI). The overall resulting N7800A measurement uncertainties then reflects these lower device uncertainties. The equipment requirements of each N7800A calibration application are summarized in the Special Calibrations Matrix which can be found at http://cal.software.keysight.com.
Option H99 is a special option for the Roseville Service Center [only] which provides electronic calibration data available as a .csv file that can then be imported into TME, thus avoiding manual entry. Option H99 must be requested from the Roseville Service Center upon re-calibration only of any previously purchased power sensor. It is not available with new purchases of power sensors. This option may be ordered in addition to any other required or requested Std Lab Calibration option. Option H99 is recommended but not required.
|
|
The following models are not supported by Option H99:
|