Frequency switching speed is defined as the time required for the DUT to switch from one frequency to another. Switching starts at the receipt of a SCPI command or trigger signal. Switching ends when the signal settles to within 100 Hz of the final frequency.
The signal generator is set to sweep mode, switching from one frequency point to another. The spectrum analyzer is set to capture the FM deviation at the stop frequency. Then, the function generator is used to simultaneously trigger both the signal generator frequency switch and the start of the spectrum analyzer’s sweep. The spectrum analyzer measures the time it takes for the signal to settle within the tolerance.
|
Test Equipment |
Critical Specifications for This Test |
Recommended Model |
Alternate Models |
|
Spectrum Analyzer |
Sweep Time Accuracy |
N9030B Opt 5xx1, MPB, and N9063EM0E Analog Demodulation Measurement application |
N9030A Opt 5xx1, MPB, and N9063EM0D Analog Demodulation Measurement application2 E444xA3 Opt 233, 23A4, and 1235 |
|
Function Generator |
|
33622A |
33611A |
|
|||
|
|
|
If this performance test fails, perform the following steps in order:
Check the equipment setup (see above). If the setup is incorrect, make the necessary corrections and rerun the performance test.
Refer to the troubleshooting section of the service guide. If you do not have a printed copy of the service guide (Option OBW), one is available either on the CD-ROM that came with your signal generator shipment or search for your signal generator model number on the Keysight website.
If necessary, obtain service from Keysight Technologies. Refer to Contacting Keysight Technologies.