The Glide Slope operates with a carrier frequency in the 329.9–335 MHz band and provides signals which indicate whether the aircraft is above, below, or on the glide path. The Glide Slope provides the same type of information as the Localizer, but for a vertical reference as opposed to a horizontal reference.
|
Test Equipment |
Recommended Model |
Alternate Model |
|
Spectrum Analyzer |
N9030B Opt 5xx1, N9063EM0E Analog Demodulation Measurement Application |
N9030A Opt 5xx1, N9063EM0D Analog Demodulation Measurement Application2 |
|
|
|
|
If this performance test fails, perform the following steps in order:
Check the equipment setup (see above). If the setup is incorrect, make the necessary corrections and rerun the performance test.
Refer to the troubleshooting section of the service guide. If you do not have a printed copy of the service guide (Option OBW), one is available either on the CD-ROM that came with your signal generator shipment or search for your signal generator model number on the Keysight website.
If necessary, obtain service from Keysight Technologies. Refer to Contacting Keysight Technologies.