Power level accuracy is the difference between the power level indicated by the device under test (PDUT), and the true power delivered by the DUT (PgZ0).
PLAdB = PgZ0 - PDUT
Direct absolute power measurements are made with a power meter for the higher powers. For lower powers, a cross-calibration is performed and remaining powers measured with the spectrum analyzer.
|
Test Equipment |
Recommended Model |
Alternate Models |
|
Power Meter |
N1914A1 |
E4419A/B |
|
Spectrum Analyzer |
N9030B Opt 5xx3, MPB, Pxx4 |
E444xA2 Opt 110 and 123 N9030A Opt 5xx3, MPB, Pxx4 |
|
Power Sensor |
E9304A E9304A Opt H19 |
N8482A N8482A CFT E9304A H18 U8481A5 Opt 200 |
|
||
|
|
|
This test uses flexible power sensor channel assignment and will identify the channel that a power sensor is connected to using the ability of "smart" sensors such as the N848xA, U848xA, and E930xA series to report their full model and serial number.
Select from the links below for connection setups depending on the power sensor.
Sometimes noise from nearby test equipment can affect low-level measurements. Errors may be caused even if the power meter is stacked on top of the spectrum analyzer.
Inspect all RF cables. If semi-rigid cables are used, check for cracks in the shielding or at the connectors. RF leakage to/from the cables generally cause problems at higher frequencies (> 2 GHz) and low power levels (< -100 dBm).
Verify that the spectrum analyzer does not have a residual spur at the frequency being measured. Sometimes a spur will limit how low in power the spectrum analyzer can measure.
Make sure that all test equipment is using the same power outlet. Ground loops can cause problems at low power levels. This type of problem will most likely show up at lower frequencies.
Make sure all covers on the DUT are secure and that all screws are in place.
Make sure all connections in the measurement system are torqued properly. Loose or damaged connections result in RF leakage and errors result at low power levels.
Make sure all test equipment
has been turned on at least 30 minutes.