VHF Omnidirectional Ranging (VOR) is a system used to guide aircraft from one location to another. VOR stations are located such that they can provide complete coverage for air traffic. Each station radiates a carrier in the 108 MHz to 118 MHz band, which is modulated in a way that provides aircraft bearing information relative to the transmitter location. There are two parts to the modulation: a 30 Hz reference signal and a 30 Hz variable phase signal.
|
Test Equipment |
Recommended Model |
Alternate Model |
|
Spectrum Analyzer |
N9030B Opt 5xx1, N9063EM0E Analog Demodulation Measurement Application |
N9030A Opt 5xx1, N9063EM0D Analog Demodulation Measurement Application2 |
|
|
|
|
If this performance test fails, perform the following steps in order:
Check the equipment setup (see above). If the setup is incorrect, make the necessary corrections and rerun the performance test.
Refer to the troubleshooting section of the service guide. If you do not have a printed copy of the service guide (Option OBW), one is available either on the CD-ROM that came with your signal generator shipment or search for your signal generator model number on the Keysight website.
If necessary, obtain service from Keysight Technologies. Refer to Contacting Keysight Technologies.