This section lists the test equipment needed to run performance tests and adjustments. Models for each test equipment category are given in order of preference. Alternate models are also listed but should be considered a lower priority. All equipment is Keysight, Agilent, or Hewlett Packard unless otherwise specified. Quantity required is one each unless specified otherwise. Refer to each individual test for specific setup configurations.
|
Test Equipment |
Recommended Model |
Alternate Model |
|
Analyzers |
||
|
Signal analyzer, Note the following: M9484C signal generators with frequency option 554 can only use the N9041B. All other VXG models can use any of the recommended or alternate models providing that the frequency option is ≥ the maximum frequency of the DUT.
|
N9041B with options: Frequency option for Input 2: 590, 90 GHz Other options:
|
N9040B With options:
(Options Pxx & MPB are used but not required by Power Level Accuracy.)
|
|
Signal analyzer,
|
N9040B with options:
|
|
|
Vector Signal Analysis Application
|
89600 VSA with licenses:
|
|
|
Sources |
||
|
Phase noise reference source
|
E8257D1 Options 5xx2, UNT, UNY,1EU
|
None |
|
Phase noise measurement system |
N5511A Options 526 or 540, CH21
|
E5505A Option 0011
|
|
Power meters and power sensors (See below for calibration service ordering guidelines.) |
||
|
Power meter Note: USB power sensors require a power meter with USB ports. |
N1914B
|
N1913B N1914A1, 2 N1912A E4419A1
|
|
Power Sensor 1 For performance verification tests for M9484C Note: USB power sensors require a power meter with USB ports. |
U8488A Option 200 |
U8487A1 Option 200
|
|
Power Sensor 1 For performance verification tests for M9384B Note: USB power sensors require a power meter with USB ports. |
U8488A Option 200 |
U8488A Option 100 U8487A Option 100 / 200 U8485A1 Option 100 / 200 N8485A1 Option 033, STD / CFT
|
|
High-Power Power Sensor For M9384B with option 1EB or 1EE for performance verification tests. |
E9300A-H25 |
None |
|
Power Sensor 1 For adjustments |
N8488A |
None |
|
Other devices |
||
|
High performance oscilloscope |
DSOZ634A1
|
Select any oscilloscope frequency option that has a maximum frequency greater than or equal to the maximum frequency of the unit under test. DSAX92004A DSOX92004A MSOX92004A DSAV204A1 DSOV204A1 DSAZ204A1 DSOZ204A1
|
|
50 Ω termination, Type-N (m)
|
909A Option 012 |
|
|
50 Ω termination, 3.5 mm (f)
|
909D |
|
|
50 Ω termination, 2.4 mm (f)
|
85138B |
|
|
Low frequency power divider |
Mini-Circuits ZFSC-2-5-S+ |
None |
|
High frequency power divider |
87303C |
None |
|
mmWave power divider
|
Marki PD-0465 |
None |
|
mmWave phase detector
|
Marki MM1-2567LS |
None |
Click below for a table that lists the various options that will provide USB ports on the N1914A power meter.
|
N1914A Orderable Options |
Description |
FW responds as option1 |
|
|
201 |
Ordered from the factory with new N1914A |
Dual channel average power meter with VGA, trigger in/out, 1 front and 1 rear USB port |
008, 010, 012 |
|
The following options are ordered as upgrades to an existing N1914A power meter. |
|||
|
106 |
This is the recommended option. |
Dual channel average power meter with 1 front and 1 rear USB port |
008 |
|
103 |
alternate |
Dual channel average power meter, battery, 2 rear USB ports |
001, 009 |
|
105 |
alternate |
Dual channel average power meter with VGA, battery, 1 front and 1 rear USB port |
008, 010 |
|
108 |
alternate |
Parallel rear-panel sensor input connectors, front-panel reference calibrator connector, 2 rear USB ports |
002, 009 |
|
109 |
alternate |
Parallel rear-panel sensor input connectors, rear-panel reference calibrator connector, 2 rear USB ports |
003, 009 |
|
111 |
alternate |
Dual channel average power meter, battery, 1 front and 1 rear USB port |
001, 008 |
|
167 |
alternate |
Dual channel average power meter, external trigger in/out, 1 front and 1 rear USB port |
008, 012 |
|
Use the following guidelines to ensure power sensors used by the N7800A application receive the correct calibration service:
Order Option 1A7 when ordering new power sensors that will be used as working standards in N7800A TME calibrations.
When ordering periodic calibration for instruments used as lab standards in the N7800A software, we recommend using “Keysight Cal + Uncertainties + Guardbanding”. More information can be found at http://www.keysight.com/find/americas_cal.
The N7800A software incorporates the ISO GUM Uncertainty in point-to-point uncertainty calculations. The special “H-series” calibration options (shown on the Special Calibrations Matrix located at http://cal.software.keysight.com) provide lower measurement uncertainties through use of direct comparison to devices directly characterized by NPL or NIST (or another NMI). The overall resulting N7800A measurement uncertainties then reflects these lower device uncertainties. The equipment requirements of each N7800A calibration application are summarized in the Special Calibrations Matrix which can be found at http://cal.software.keysight.com.
Option H99 is a special option for the Roseville Service Center [only] which provides electronic calibration data available as a .csv file that can be imported into TME thus avoiding manual entry. Option H99 must be requested from the Roseville Service Center upon re-calibration only of any previously purchased power sensor and not for new purchases of power sensors. This option may be ordered in addition to any other required or requested Std Lab Calibration option. Option H99 is recommended but not required.
|
|
The following models are not supported by Option H99:
|