|
This test measures the Timebase by dividing the sample clock by 10 (within the meter) and feeding it out of the Trigger Output connector, where it can be directly measured by a frequency counter.
|
Test Equipment |
Recommended Model Number1 |
|
Universal Frequency Counter |
53230A |
|
10 MHz Frequency Standard |
Microsemei 5071A |
|
BNC cable |
8120-2582 |
|
Adapter, SMB (f) to BNC (f) |
1250-1236 |
|
|
Connections on power meters with rear panel options will differ than those in the illustrations below. Refer to the rear panel of the power meter for connector identification labels. |