|
|
|
N5221B, N5222B, N5224B, N5225B, N5227B with Option 090 plus one of the spectrum analyzer frequency options (shown below) and <RSA> (see below for <RSA> explanation)
N5231B, N5232B, N5234B, N5235B, N5239B with Option 090 plus one of the spectrum analyzer frequency options (shown below) and <RSA> (see below for <RSA> explanation)
N5241B/BC, N5242B, N5244B, N5245B/BC, N5247B/BC, N5249B with Option 090 plus one of the spectrum analyzer frequency options (shown below) and <RSA> (see below for <RSA> explanation)
N5290A, N5291A mm-Wave systems with Option 090 plus one of the spectrum analyzer frequency options (shown below) and <RSA> (see below for <RSA> explanation)
This test generates a report that is based on part of the Calibration Coefficients test. Therefore, the Calibration Coefficients test must be completed prior to running this test. TME will check if the Calibrations Coefficients test has been run within the allowed time period. If not, the user will be instructed to run the Calibrations Coefficients test prior to running the VSWR test.
N52xxB, N5290A, and N5291A models with Option 090 (spectrum analysis application) also require one of the following spectrum analyzer frequency options. TME will test to the maximum frequency of the DUT OR the spectrum analyzer frequency option range, whichever is lowest.
|
900 — up to 8.5 GHz |
|
901 — up to 13.5 GHz |
|
902 — up to 26.5 GHz |
|
904 — up to 43.5 GHz |
|
905 — up to 50 GHz |
|
907 — up to 67 GHz |
|
909 — up to 90 GHz |
|
093 — extend to 110 GHz |
|
094 — extends beyond 110 GHz |
This section will explain how to determine if your model requires Option <RSA> for this test.
Some models require Option <RSA> for this test. Options in angle brackets (such as <RSA>) are assigned by TME to facilitate testing and do not reflect product options. For this reason, Option <RSA> will not appear on reports or other places of the TME User Interface.
The following models require Option <RSA> to run this test:
N5221B, N5222B, N5224B, N5225B, N5227B
N5231B, N5232B, N5234B, N5235B, N5239B
N5241B/BC, N5242B, N5244B, N5245B/BC, N5247B/BC, N5249B
N5290A, N5291A
None