|
|
Power meters with firmware version A2.03.00 (or A1.03.00) may not operate properly with the new test software. Upgrade the power meter firmware if necessary. |
Review the General Troubleshooting recommendations before proceeding with this section.
A failure in this test may indicate a need to correct the source flatness. This is accomplished by performing the Source Calibration Adjustment. If the source power accuracy is still out of specification after performing the adjustment, troubleshoot the source hardware chain. Refer to the appropriate PNA service guide for information.
You should not see a source unlevelled error reported on the PNA display during this test. If this error occurs and the test fails, first fix the source unlevelled problem.