Frequency Accuracy Adjustment

This adjustment applies to the following models:

  • This adjustment requires a 90 minute warmup period.
  • This adjustment requires Option CFG. Refer to the CFG Option topic for more information.

This adjustment selects the DAC setting that gives the best frequency accuracy when using the analyzer's internal reference. The DAC used for internal reference is also used for locking to an external frequency reference. The adjustment algorithm simply requests the instrument to lock to the external 10 MHz provided by the 10 MHz frequency standard, and then reads the DAC setting which has been set by the firmware locking algorithm.

The DAC value is averaged and this average DAC value is stored for the adjustment. The average value is compared to limits. The highest and lowest DAC values are checked to ensure that the firmware was properly locking.

Related test:

Frequency Accuracy

Required Test Equipment

Test Equipment

Recommended Model Number
(see main equipment list for alternative models)

Freqency Standard

Microsemi 5071A

Cable, BNC

8120-2582

 

Connection Setup