CFG Option

Refer to the section below for a list of FieldFox model/option combinations that require a CFG Option.

Some FieldFox model and option combinations will require the installation of the CFG Option in order to complete certain tests, adjustments, and utilities. This option ensures that all SCPI commands required to successfully run tests and adjustments are enabled in the FieldFox analyzer. Installation of the CFG Option does not modify the performance of the FieldFox analyzer nor does it change the test results.

If a test or adjustment requires the CFG Option, TME will verify if the option is installed. If the CFG Option is required but not installed, TME will display a dialog box. Below is an example. Note that the tests or adjustments listed in the dialog box will vary depending on model and option combinations.

CFG Option Dialog Box Example

Obtaining and Installing a CFG Option License

  • Refer to the section below for a list of FieldFox model/option combinations that require a CFG Option.

  • Instructions in previous versions of the Help regarding obtaining an OEC (Option Entitlement Certificate) and redeeming licenses using KSM (Keysight Software Manager) are no longer valid. An OEC is not required to obtain a CFG option license.

  • Before installing a CFG option, check the time, date, and time zone. Refer to the instrument's user's guide for instructions on changing the date and clock of the FieldFox.

Follow the steps below to obtain and install a CFG option license.

  1. To obtain a CFG option license, send an email to the service desk with the FieldFox model and serial number requesting a CFG option license. A license will be emailed to you. The service desk email address is: csg.servicedesk@keysight.com

  2. Copy the license file from the email to the root directory of a USB flash drive that is formatted in FAT32.

  3. Insert the USB flash drive into the FieldFox, then press System (7) > System Configuration > Options > Install Options

    The instrument reads the license file from the USB flash drive, validates the file, and installs the CFG option.

  4. Disconnect the USB flash drive from the FieldFox.

  5. Cycle power on the instrument to activate the newly installed option. (Hold the power button down for more than four seconds to completely power down the instrument.)

  6. View the installed option upgrade(s). On the FieldFox press System (7) > System Configuration > Options > Show Options

  7. Once testing is complete, remove the CFG license prior to returning the unit to the customer. Follow the instructions in the next section.

Removing a CFG License

For a given FieldFox instrument, a CFG license enables functionality not licensed for normal use. It is important to remove CFG license(s) from a FieldFox prior to returning the unit to a user.

To remove CFG license(s) from a FieldFox instrument, follow the steps below:

  1. Press System > System Configuration > Options (Licensing) > Advanced

  2. Press Delete All CFG Options and then confirm.

  3. It is assumed the unit will be powered off prior to returning to the user.

CFG License Notes

When a CFG Option Is Needed

Tests

The following model/option combinations require a CFG license to complete testing:

Models

Option Configuration

N9912A

230/231 missing but 311 present

303 missing

N9923A

122 missing

N9913A/B, N9914A/B, N9915A/B, N9916A/B, N9917A/B, N9918A/B

210 missing

211 missing but 210 present

233 missing but 310 present

N9925A, N9926A, N9927A, N9928A

211 missing

310 present

N9933B, N9934B, N9935A/B, N9936A/B, N9937A/B, N9938A/B

320 present

220 present

N9950A, N9951A, N9952A

210 missing

211 missing but 210 present

233 missing but 310 present

N9960A, N9961A, N9962A

320 present

220 present

 

Adjustments

The following model/option combinations require a CFG license to complete all required adjustments:

Models

Option Configuration

N9912A

All model and option combinations.

N9923A

All model and option combinations.

N9913A, N9914A, N9915A, N9916A, N9917A, N9918A

All model and option combinations.

N9925A, N9926A, N9927A, N9928A

All model and option combinations.

N9935A, N9936A, N9937A, N9938A

All model and option combinations.

N9950A, N9951A, N9952A

All model and option combinations.

N9960A, N9961A, N9962A

All model and option combinations.

 

Utilities

The following model/option combinations require a CFG license for the indicated procedure:

Models

Option Configuration

Affected Utility Procedure

N9912A

303 missing

ECal Error Terms Adjustment (Utility)

N9923A

122 missing

ECal Error Terms Adjustment (Utility)

N9913A/B, N9914A/B, N9915A/B, N9916A/B, N9917A/B, N9918A/B

233 missing

Source Isolation Utility

N9925A, N9926A, N9927A, N9928A

 

N9933B, N9934B, N9935A/B, N9936A/B, N9937A/B, N9938A/B

220 missing

N9950A, N9951A, N9952A

233 missing

N9960A, N9961A, N9962A

220 missing