Spectrum Analyzer Adjustment

This adjustment applies to the following models:

This adjustment requires Option CFG. Refer to the CFG Option topic for more information

The Spectrum Analyzer Adjustment consists of five different adjustments that are run sequentially as the Spectrum Analyzer Adjustment. The adjustment uses two different equipment setups. Part one of the procedure will use a calibrated PNA-X for frequencies above 15 MHz. The second part of the adjustment will use a function generator for frequencies from 9 kHz to 15 MHz.

Part One: Frequencies Above 15 MHz

This part of the Spectrum Analyzer Adjustment will run the following adjustments using a calibrated network analyzer:

  1. Absolute Amplitude
  2. Frequency Response (Band 2 and greater)
  3. Attenuator Slope (Band 2 and greater)
  4. IF Frequency Response (Band 2 and greater)

ClosedClick here for equipment setup details.

Part Two: Frequencies 9 kHz to 15 MHz

This part of the Spectrum Analyzer Adjustment will run the following adjustments using a function generator:

  1. LO Feedthru
  2. Frequency Response (Band 1 only)
  3. Attenuator Slope (Band 1 only)
  4. IF Frequency Response (Band 1 only)

ClosedClick here for equipment setup details: