N9935A/36A/37A/38A
|
|
All adjustments will require the CFG Option. Refer to the CFG Option section for more information. |
For Fieldfox analyzers with firmware A.09.00 and above, TME will run the five spectrum analyzer adjustments as one "super" adjustment called the Spectrum Analyzer Adjustment. The adjustment uses two different equipment setups. Part one of the procedure will use a signal generator for frequencies above 15 MHz. The second part of the adjustment will use a function generator for frequencies from 9 kHz to 15 MHz.
This part of the Spectrum Analyzer Adjustment will run the following adjustments using a signal generator:
IF Frequency Response
Click here for equipment setup details.|
Test Equipment |
Recommended Model Number |
|---|---|
|
Signal Generator #1 |
E8257D with options:
|
|
Power Meter |
N1914A |
|
Power Sensor
|
E9304A Option H20 |
|
Power Sensor
|
N8485A |
|
Power Sensor
|
8485D |
|
Attenuator, 30 dB
|
11708A |
|
Power Splitter, 3.5 mm |
11667B |
|
Power Sensor Cable |
11730A |
|
BNC Cable |
8120-2582 |
|
Coaxial Cable |
11500E |
|
Adapter, 3.5 mm (m) to Type-N (m) |
1250-1743 |
|
Adapter, 3.5 mm (f) to 3.5 mm (f)
|
83059B |
|
Adapter, 2.4 mm (f) to 3.5 mm(f)
|
11901B |
|
|
|
|
|
The following notes apply to illustrations in the FieldFox Help:
|
Click here for Frequency Response power meter/sensors calibration and splitter characterization setups.
This part of the Spectrum Analyzer Adjustment will run the following adjustments using a function generator:
IF Frequency Response
Click here for equipment setup details:|
Test Equipment |
Recommended Model Number |
|---|---|
|
Function Generator |
33622A |
|
Power Meter |
N1914A |
|
Power Sensor |
E9304A Opt H20 |
|
Power Splitter |
11667B |
|
Power Sensor Cable |
11730A |
|
BNC Cable |
8120-2582 |
|
Coaxial Cable |
11500E |
|
Adapter, 3.5 mm (m) to Type-N (m) |
1250-1743 |
|
|
The following notes apply to illustrations in the FieldFox Help:
|