This section lists the required test equipment for the following the PNA series network analyzers:
2-port RF network analyzers
|
3-port RF network analyzers
|
|
Test Equipment1 |
Recommended Model |
Alternate Model |
|
Sources |
||
|
Signal Generator Only used with the U3020A-D01 test set in the Dynamic Accuracy test. |
E8257D |
N5182B |
|
Counters |
||
|
Frequency Counter |
53230A Option 115 |
53131A/32A Options 010, 012, 1242 53181A Options 010, 1242 |
|
Meters and Power Sensors (See below for calibration service ordering guidelines.) |
||
|
N1914A5 |
E4419A/B |
|
|
Power Sensor 6 |
8482A |
|
|
8481A |
||
|
Attenuators |
||
|
10 dB Fixed 8 |
8491A Option 010 |
8491B Option 010 |
|
20 dB Fixed 8 |
8491A Option 020 |
8491B Option 020 |
|
Miscellaneous Devices |
||
|
Dynamic Accuracy Test Set |
U3020A-D01 |
Z5623A Option H01 |
|
Load 3.5 mm (m) May come from 85058B cal kit |
909D |
902C |
|
Type-N Calibration Kit |
85032F |
85032B (not for 9 GHz PNAs) |
|
USB Mouse |
Any |
Any |
|
USB Keyboard |
Any |
Any |
|
Cables |
||
|
RF Type-N (m) to Type-N (m) (2 required) |
N6314A |
8120-8862 |
|
BNC RF |
Any |
Any |
|
GPIB |
10833A/B/C/D |
Equivalent |
|
Power sensor cable 3 |
11730A |
Equivalent |
|
Adapters |
||
|
Type-N (f) to Type-N (f) |
1250-0778 |
Equivalent |
|
Type-N (m) to Type-N (m) |
1250-0777 |
Equivalent |
|
BNC (m) to Type-N (f) |
1250-1477 |
Equivalent |
|
Static Safety Equipment |
||
|
Adjustable antistatic wrist strap |
9300-1367 |
None |
|
Antistatic wrist strap grounding cord (5 foot) |
9300-0980 |
None |
|
Static control table mat and earth ground wire |
9300-0797 |
None |
|
Use the following guidelines to ensure power sensors used by the N7800A application receive the correct calibration service:
Order Option 1A7 when ordering new power sensors that will be used as working standards in N7800A TME calibrations.
Order the Keysight Cal + Measurement Uncertainty + GB calibration service for power sensor recalibration.
When ordering periodic calibration for instruments used as lab standards in the N7800A software, we recommend using “Keysight calibration + uncertainties” for power sensors, and “Keysight calibration + uncertainties + guardbanding” for all other items (please visit Selecting the Right Calibration Services). The N7800A software incorporates the ISO GUM Uncertainty in point-to-point uncertainty calculations. The special “H-series” calibration options in this table provide lower measurement uncertainties through use of direct comparison to devices directly characterized by NPL or NIST (or another NMI). Please order Option H99 to get electronic data for easy import into the N7800A (avoids manual entry). The overall resulting N7800A measurement uncertainties then reflects these lower device uncertainties. The equipment requirements of each N7800A calibration application are summarized in the specials calibration matrix which can be found at the Recommended Lab Standards and Special Cal Options website.
The Keysight Option H99 is a special option for the Roseville Service Center [only] which provides electronic calibration data available as a .csv file in TME N7800A format for all power sensors used with the N7800A TME application. N7800A TME is SSU calibration software used across Keysight SSU and by many self-maintainers. H99 must be requested from the Roseville SSU upon re-calibration only of any previously purchased power sensor and not for new purchases of BID Power Sensors. This option may be ordered in addition to any other required or requested Std Lab Calibration option (must also be ordered in addition to H99). Option H99 is recommended but not required.