8485D
This is a functional test and only applies to power sensors that do not have EEPROM. This test stores the calibration factors generated in the Calibration Factor test to an XML file, which can be used as the original calibration factors in the Calibration Factor Deviation test in the next calibration cycle.
The XML file will be stored at:
C:\ProgramData\Keysight\PowerSensor\CalFactorDeviation\TempCF\{Model#}_{Serial#}.xml
If there is an existing file with the same name, it will be renamed to {Model#}_{Serial#}pre.xml.