This test measures the Voltage Standing Wave Ratio (VSWR) of the Keysight power sensor. A network analyzer accompanied with a calibration kit or electronic calibration modules is used to perform this test.
For the UUT N848xB power sensors, the network analyzer calibration is done in the Two Port Network Analyzer Calibration test.
|
|
To view the table below in its entirety, you may need to select the Hide Navigation button from the toolbar. |
| Instrument | Recommended product | Alternative product | N8481A (all except Opt 200), 8481A, N8481B, N8481H | N8481A Opt 200 | N8482A, 8482A, E9304A, N8482B, N8482H (all except Opt Z2092B-208) |
N8482A, 8482A, E9304A, N8482B, N8482H (Opt Z2092B-208) |
N8485A (all except Opt 033), 8485A | N8485A Opt 033 | 8485D | 8487A, N8487A | E9304A Opt H18[1] | E9304A Opt H18, Z2092B-208 | N8486AR | N8486AQ | N8488A |
| Network analyzers | |||||||||||||||
| PNA[2] | N5247B |
N5247A/AS E8361C |
X | X | X | X | X | X | X | X | X | X | X |
X Alternative models: N5247A/AS |
|
| ENA | E5071C[4] | - | X | X | |||||||||||
| Calibration Kits/Electronic Calibration Modules | |||||||||||||||
| 50 Ω Calibration Kit Type-N for Network Analyzer |
85054B |
Electronic Calibration Module N4690B Opt M0F Electronic Calibration Module N4690D[5] Opt M0F |
X Except UUT N848xB |
X | X | ||||||||||
| 50 Ω Calibration Kit 7 mm for Network Analyzer |
85050B | - | X | ||||||||||||
| 50 Ω Calibration Kit Type-N for Network Analyzer |
85032F | - |
X Except UUT N848xB |
X Except UUT N848xB Alternative ECal Module: N4690B Opt M0F, N4690D[5] Opt M0F, or Calibration Kit 85054B |
X | ||||||||||
| 50 Ω Calibration Kit 3.5 mm for Network Analyzer |
85052B | Electronic Calibration Module N4691B Opt M0F Electronic Calibration Module N4691D[5] Opt M0F |
X | X | |||||||||||
| 50 Ω Calibration Kit 2.4 mm for Network Analyzer |
85056A | Electronic Calibration Module N4693A Opt M0F Electronic Calibration Module N4693D[5] Opt M0F |
X | ||||||||||||
| 1 Ω Calibration Kit | R11644A |
- | X | ||||||||||||
| 1 Ω Calibration Kit | Q11644A | - | X | ||||||||||||
| Electronic Calibration Module 3.5 mm for Network Analyzer |
N4691BH33 Opt M0F | - |
X | ||||||||||||
| Electronic Calibration Module 1.85 mm for Network Analyzer |
N4694D[5] Opt M0F | N4694A Opt M0F N4694A Opt 00M |
X | ||||||||||||
| Load | 85058-60111 use with N4694A Opt M0F/N4694D[5] Opt M0F | 85058-60112 use with N4694A Opt 00M |
X | ||||||||||||
| Meter | |||||||||||||||
| Power Meter | N1914B | N1914A E4419B N1912A |
X Except UUT 8481A |
X | X |
X |
X Except UUT 8485A |
X | X |
X Except UUT 8487A |
X | X | X | X | X |
| Power Sensors[6]/Verification Kits | |||||||||||||||
| Power Sensor | N8481A |
8481A or N8481B or N8481Hor 8481B or 8481H or Verification Kit 85055A | X | ||||||||||||
| Power Sensor | N8481A Opt 200 |
8481A Opt 001 or Verification Kit 85051B (45 MHz to 18 GHz only) | X | ||||||||||||
| Power Sensor | N8482A | E9304A or 8482A (For UUT 8482A only) or N8482B or N8482H or Verification Kit 85055A (300 kHz to 6 GHz only) |
X For UUT E9304A, Recommended product: E9304A (9 kHz to 6 GHz) Alternative product: 85055A (300 kHz to 6 GHz) |
X For UUT E9304A, Recommended product: E9304A (9 kHz to 6 GHz) Alternative product: 85055A |
|||||||||||
| Power Sensor | N8485A | 8485A or Verification Kit 85053B | X | ||||||||||||
| Power Sensor | N8485A Opt 033 | 8485A Opt 033 | X | ||||||||||||
| Power Sensor | 8485D | Verification Kit 85053B | X | ||||||||||||
| Power Sensor | N8487A | 8487A or Verification Kit 85057B |
X | ||||||||||||
| Power Sensor | E9304A Opt H18 | Verification Kit 85055A (300 kHz to 18 GHz) | X | X | |||||||||||
| Power Sensor | N8486AR |
R8486A |
X | ||||||||||||
| Power Sensor | N8486AQ | Q8486A | X | ||||||||||||
| Power Sensor | N8488A | - | X | ||||||||||||
| Adapters | |||||||||||||||
| 2.4 mm (f) to Type-N (f) | 11903B |
- | X | X | X | X | |||||||||
| 2.4 mm (f) to APC-7 | 11902B |
- | X | ||||||||||||
| 2.4 mm (f) to 3.5 mm (f) | 11901B |
- | X | X | X | ||||||||||
| 2.4 mm (f) to 2.4 mm (f) | 11900B | 85056-60006 (Shipped with the Calibration Kit 85056A) |
X | X | X | ||||||||||
| WR-28 to 2.4mm (m) |
R281B |
- | X | ||||||||||||
| WR-22 to 2.4 mm (m) | Q281B | - | X | ||||||||||||
| 1.85 mm (F) to 1.85 mm (F) | 85058-60008 | 85058-60121 | X | ||||||||||||
[1] E9304A Opt H18 uses both ENA and PNA to perform VSWR test. ENA covers 9 kHz to < 10 MHz and PNA covers 10 MHz to 18 GHz frequency range.
[2] The following minimum PNA firmware revisions or above are required to include phase wrapping fix:
[3] Supported N5230A and N5230C options: This calibration application supports any option that covers the entire frequency range of the UUT.
[4] Supported E5071C options: This calibration application supports any option that covers the entire frequency range of the UUT.
[5] D-model ECals can only be used with the following network analyzer models and firmware versions:
[6] Supported power sensor options:
|
|
When connecting the power sensor model N8481B or N8482B to the network analyzer’s test port, please ensure the fixed attenuator is supported by an object or fixture to prevent bending on the adapter or connector. See the picture below for an example of the connection.
|
The Verification Kit can be used instead of a power sensor to verify the network analyzer calibration. The software will only use one item in the Verification Kit to verify the calibration — this item will be the largest fixed attenuator in the kit.
Each Verification Kit comes with a 3.5 floppy PNA Verification Data Disk or a USB flash disk which contains the data we need to verify the network analyzer calibration.
In order to use the verification kit, save the .unc and .dat file for the largest fixed attenuator to this location:
C:\Documents and Settings\All Users\Application Data\Agilent Technologies\Test Management Environment\VerificationKit
You will need to rename the file by opening the file and copying from the second line everything that follows “#Part: “ This number contains the model number and serial number of the fixed attenuator. When mapping the verification kit in TME, enter the 5 digit serial number located on the largest fixed attenuator in the kit.
Copy the files here:
Open the file and copy the part number:
Rename the files using the part number:
An E-Cal may be used for the Network Analyzer Calibration instead of a mechanical calibration kit. When using the E-Cal, connect it to the network analyzer using a USB cable. Before using the E-Cal, ensure that the ready light has turned green on the unit. When mapping the E-Cal in TME, the serial number should be a 5 digit number with no letters. If there is no five-digit serial number printed on your unit, then follows these instructions using your network analyzer to locate your serial number:
For all UUT models, except N8486AR and N8486AQ:
For UUT models N8486AR and N8486AQ:
For UUT models N8488A:
For all verification sensors, except 8485D, E9304A, and E9304A Opt H18:
For verification sensor 8485D, E9304A, and E9304A Opt H18:
For verification sensor N8486AR and N8486AQ:
For all UUT, except 8485D, E9304A, and E9304A Opt H18:
For UUT 8485D, E9304A, and E9304A Opt H18:
For UUT N8486AR and N8486AQ:
For UUT N8481B and N8482B: