This section lists the test equipment needed to run performance tests. Refer to each individual test for specific setup configurations with required cables and adapters. Not all of the listed test equipment needs to be connected to perform an individual test. To run a test, only the equipment specified for that test needs to be connected.
|
|
In all test equipment configurations, cables and adapters must be properly torqued. Exceeding recommended torque values can cause damage to a cable or adapter, and can cause inaccurate test results. |
| To make this connection | Use this driver or torque wrench and torque value |
N8481A (all except Opt 200), N8481B, N8481H, 8481A, N8482A, N8482B, N8482H, 8482A, N8487A, 8487A, N8488A, E9304A, E9304A Opt H18 |
N8481A Opt 200 | N8485A, 8485A, 8485D | N8486AR, N8486AQ |
| 3.5 mm (m) to 3.5 mm (f) 2.4 mm (m) to 2.4 mm (f) |
8710-1765 (8 lb-in, 5/16 inch open end) |
X | X | X | |
| 3.5 mm (m) to 3.5 mm (f) | 8710-1764 (8 lb-in, 20 mm open end) |
X | |||
| Type-N (m) to Type N (f) | 8710-1766 (12 lb-in, 3/4 inch open end) |
X | X | ||
| APC-7 to APC-7 | 8710-1766 (12 lb-in 3/4 inch open end) |
X | |||
| Waveguide flange UG-383/U or Waveguide flange UG-599/U |
8710-0523 |
X | |||
|
1. The Balldriver is used to tighten the screws, instead of the connector. |
|||||
|
|
|
| Instrument | Recommended product | Alternative product |
| Signal Sources | ||
| Signal Generator | E8257D Opt 1E1, IEU/1EA, and [550 or 567] | - |
| Function Generator | 33622A |
33612A |
| Power Supply | N5745A | E3632A (Except N8480H) |
| Power Supply | 87422A | - |
| Network Analyzers | ||
| PNA | N5247B |
N5247A/AS E8361C |
| ENA | E5071C2 | - |
| Calibration Kits/Electronic Calibration Modules | ||
| 50 Ω Calibration Kit | 85054B |
N4690B Opt M0F N4690D3 Opt M0F |
| 50 Ω Calibration Kit | 85032F | N4690B Opt M0F, N4690D3 Opt M0F, or 85054B (50 MHz Cal Port VSWR and VSWR tests only — specific UUT models only) |
| 50 Ω Calibration Kit | 85052B | N4691B Opt M0F N4691D3 Opt M0F |
| 50 Ω Calibration Kit | 85056A | N4693A Opt M0F N4693D3 Opt M0F |
| 50 Ω Calibration Kit | 85050B | - |
| 1 Ω Calibration Kit | R11644A | - |
| 1 Ω Calibration Kit | Q11644A | - |
| Electronic Calibration Module | N4691BH33 Opt M0F | - |
| Electronic Calibration Module | N4694D3 Opt M0F | N4694A Opt M0F N4694A Opt 00M |
| Meters/Verification Kits | ||
| Power Meter |
N1914B |
|
| Power Sensor (3 required) 7, 8 |
N8481A | 8481A or 85055A Verification Kit (VSWR test only)9 |
| Power Sensor (3 required) 7 |
N8481A Opt 200 | 8481A Opt 001 or 85051B Verification Kit (VSWR test only) |
| Power Sensor (3 required) 7, 8 |
N8482A |
Calibration Factor test: 8482A Linearity test: 8481A Frequency range: 50 MHz VSWR test: E9304A, 8482A, N8482B, N8482H or 85055A Verification Kit Frequency range: 300 kHz to 6 GHz only |
| Power Sensor (3 required) 7, 8 |
N8485A | 8485A or 85053B Verification Kit (VSWR test only) |
| Power Sensor (3 required) 7 |
N8485A Opt 033 | 8485A Opt 033 |
| Power Sensor (3 required) 7 |
8485D | 85053B Verification Kit (VSWR test only) |
| Power Sensor (3 required) 7, 8 |
N8487A | 8487A or 85057B Verification Kit (VSWR test only) |
| Power Sensor (3 required) 7, 8 |
N8488A | - |
| Power Sensor (3 required) 7 |
E9304A | 85055A Verification Kit Frequency range: 300 kHz to 6 GHz only (VSWR test only) |
| Power Sensor (3 required) 7 |
E9304A Opt H18 | 85055A Verification Kit Frequency range: 300 kHz to 18 GHz only (VSWR test only) |
| Power Sensor (3 required) 7 |
N8486AR |
R8486A |
| Power Sensor (3 required) 7 |
N8486AQ |
Q8486A |
| Power Sensor (3 required) 7, 8 |
N8481H |
8481H |
| Power Sensor (3 required) 7, 8 |
N8482H | 8482H (Frequency range: 100 kHz to 50 MHz) and 8481H (Frequency range: 50 MHz to 6 GHz) |
| Power splitters8 | ||
| Splitter | 11667A |
- |
| Splitter | 11667A Opt 002 | - |
| Splitter | 11667B | - |
| Splitter | 11667C | - |
| Splitter | 11667CH65 | - |
| Adapters | ||
| 2.4 mm (f) to Type-N (m) |
11903D |
- |
| 2.4 mm (f) to Type-N (f) | 11903B | - |
| 2.4 mm (f) to 3.5 mm (f) | 11901B | - |
| 2.4 mm (f) to APC-7 | 11902B | - |
| Type-N (m) to BNC (m) | 1250-1473 |
- |
| 3.5 mm (f) to Type-N (m) (2 required) |
1250-1744 | - |
| 2.4 mm (f) to 3.5 mm (m) | 11901D |
- |
| Type-N (m) to Type-N (m) |
85032-60019 |
- |
| Type-N (m) to Type-N (f) adapter | 33391C-K38 | - |
| 3.5 mm (f) to Type-N (m) | 08485-60005 | - |
| 2.4 mm (f) to Type-N (m) | 08487-60001 | - |
| 2.4 mm (f) to 2.4 mm (f) | 85056-60006 | 11900B |
| APC-7 to Type N (m) (2 required) |
85054-60032 | 11525A |
| WR-28 to 2.4mm (m) | R281B | R281A (Calibration Factor test only) |
| WR-22 to 2.4 mm (m) | Q281B | R281A (Calibration Factor test only) |
| 1.85 mm (f) to 1.85 mm (f) | 85058-60008 | 85058-60121 |
| Attenuators | ||
| 3 dB High Power Fixed Attenuator | Aeroflex 40-3-43 |
- |
| 10 dB High Power Fixed Attenuator | Aeroflex 40-10-43 | - |
| 3 dB Fixed Attenuator |
8491A Opt 003 |
8491B Opt 003 |
| 6 dB Fixed Attenuator (3 required) |
8491A Opt 006 | 8491B Opt 006 |
| 10 dB Fixed Attenuator | 8491B Opt 010 | 8491A Opt 010 |
| 20 dB Fixed Attenuator | 8491B Opt 020 | 8491A Opt 020 |
| 30 dB Attenuator | 11708A | - |
| 10 dB Step Attenuator |
8496G |
- |
| 1 dB Step Attenuator | 8494G | - |
| Attenuator Driver | 11713B | 11713A |
| Miscellaneous devices | ||
| Directional Coupler |
Pulsar Microwave Corporation C4-P4-411 |
- |
| WG22 Multihole Directional Coupler (For N8486AR Calibration Factor test) |
Flann Microwave 22132-10 |
- |
| WG23 Multihole Directional Coupler (For N8486AQ Calibration Factor test) | Flann Microwave 23136-10 | - |
| Directional Bridge |
86205A | - |
| Amplifier (For N8480H linearity test) |
Mini Circuit ZHL-100W-52 |
- |
| Amplifier (For linearity test of all sensors except N8480H) |
Mini Circuit ZHL-1-2W-N |
- |
| Low Frequency Power Amplifier (For N8480[B|H] calibration factor test) |
R&K Company Limited A3000-2H-R |
- |
| High Frequency Power Amplifier (For N8480[B|H] calibration factor test) |
83020A | - |
| Filter | RLC Electronics BPF-750-50-10-5-N |
Low Pass Filter 0955-0306 and BNC (plug-m) to Type-N (f) 1250-1477 and BNC (jack-f) to Type-N (m) 1250-1476 |
| Load | 85058-60111 use with N4694A Opt M0F/N4694D3 Opt M0F | 85058-60112 use with N4694A Opt 00M |
| Label Printer | TLP 3842 (for N8480x Series Opt CFT only) |
Zebra Xi Series (for 8480 Series and N8480x Series only) |
| Cables | ||
| Type-N (m to m) (3 required) |
11500C | - |
| Wire (from Power Supply to Amplifier) |
- | - |
| 2.4mm (f) to 2.4mm (f) |
Huber and Suhner |
8120-6164 |
| 3.5mm (m) to 3.5mm (m) |
11500E |
- |
| 3.5mm(m) to 3.5mm(m) (2 required) |
5062-6656 | - |
N5230A and N5230C Options: The calibration application supports any option that covers the entire frequency range of the DUT.
E5071C Options: This calibration application supports any option that covers the entire frequency range of the UUT.
D-model ECals can only be used with the following network analyzer models and firmware versions:
N5245A/AS, N5247A/AS: Firmware version ≥ A.10.60.04
N1914A power meters with serial number prior to MY53040007 require Service Note N1914A-07 which fixes a power supply ground loop. The ground loop injects noise into the measurement circuits which can cause unstable measurements at low (-30 dBm) power levels.
N1914A power meters require minimum firmware version A.01.15 or above to fix a power linearity accuracy issue.
N1912A power meters require minimum firmware version A.05.10 or above to fix a power linearity accuracy issue.
For each power sensor model, three units are required to be used as the test equipment below:
Buried power sensor
Supported power sensor options:
8485A*: Standard Option or 033
*Power sensor Opt 033 is required if the UUT is the N8485A Opt 033.
|
|
When ordering a new STD or CFT Power Sensor from Keysight to be used with the N7800A Series applications, order with Option 1A7. The 1A7 option provides an ISO17025 calibration and includes calibration data. When re-calibrating your STD or CFT power sensor for use with the N7800A Series applications, we recommend the Keysight ISO17025 calibration. |
Refer to Required Calibration Data section for the calibration options that meet the TME requirement on the test equipment’s calibration data.
Refer to the individual performance test help for more power sensor models supported.
To ensure data integrity for measurements carried out with Test Management Environment (TME), the following verification checks are carried out at the beginning of each test run. The checks are only performed on devices that require calibration data which directly affect the test results. If you are unable to meet the calibration requirements for these devices contributing to the measurement uncertainty only, you may still produce valid reports using the standard report format option which does not contain any measurement uncertainty information.
|
|
You are still required to enter calibration factors other than the default, but uncertainty related data is not required to produce standard format reports. |
The following table lists the standard checks performed by default:
| Device | Parameter name and description | Limits | A failure affects: |
| Power Sensor | CalFactor (%)
The calibration factor, as a percentage |
Must be ≥10% and ≤150% at all points Must not be 100% (the default) at all points |
All tests that require a power sensor |
| Uncertainty (%)[1]
The uncertainty of the calibration factor, as a percentage |
Must be >0 and ≤10% at all points | Tests that require a power sensor are also guard-banded by measurement uncertainty | |
| Reflection Coefficient Magnitude
The magnitude of the reflection coefficient |
Must be >0 and <0.5 at all points | Tests that require a power sensor are also guard-banded by measurement uncertainty |
|
| Reflection Coefficient Phase (Degree)
The phase of the reflection coefficient, as a degree |
Must be ≥–180° and ≤180° at all points Must not be 0° (the default) at all points |
All tests that require a power sensor, except for Linearity test | |
| Reflection Coefficient Uncertainty
The uncertainty of the reflection coefficient magnitude |
Must be non-zero at all points | Tests that require a power sensor are also guard-banded by measurement uncertainty |
|
| Reflection Coefficient Phase Uncertainty (+/– Degree)
The uncertainty of the reflection coefficient phase, as a degree |
Must be >0° and ≤180° at all points | Tests that require a power sensor are also guard-banded by measurement | |
| Power Splitter (Port 2)[2] |
Source Match The magnitude of the equivalent source match |
Must be >0 and ≤0.5 at all points |
All tests that require a power splitter |
| Source Match Phase (Degree)
The phase of the equivalent source match, as a degree |
Must be ≥–180° and ≤180° at all points Must not be 0° (the default) at all points |
All tests that require a power splitter | |
| Source Match Uncertainty The uncertainty of the equivalent source match magnitude |
Must be non-zero | Tests that require a power splitter are also guard-banded by measurement uncertainty | |
| Source Match Phase Uncertainty (Degree)
The uncertainty of the equivalent source match phase, as a degree |
Must be >0° and ≤180° at all points | Tests that require a power splitter are also guard-banded by measurement uncertainty |
1) TME expects the power sensor calibration factor uncertainty to be absolute uncertainty.
2) The calibration data needed for power splitter is the Port 2 data. In the Calibration Factor test, the physical port of the power splitter with the Port 2 calibration data should be the test port which will be connected to Standard Power Sensor, Verification Power Sensor, or UUT.
|
|
Failure to comply with the Calibration Factor (%), Reflection Coefficient, Reflection Coefficient Phase (Degree), Source Match or Source Match Phase (Degree) limits will result in the test data being labeled Invalid in both the TME interface and any report format produced from the data. Failure to comply with the Cal Factor Uncertainty (%), Reflection Coefficient Uncertainty, Reflection Coefficient Phase Uncertainty (Degree), Source Match Uncertainty or Source Match Phase Uncertainty (Degree) limits will result in the data being labeled Invalid in the TME interface if Guard-banding is On, and in any report format, other than standard, produced from the data. If the Reflection Coefficient Phase Uncertainty (Degree) or Source Match Phase Uncertainty (Degree) is not available, please keep the default value ”0”. The application will calculate the worst case phase uncertainty and uses it to calculate the overall uncertainty. |
When running a test that required the calibration data, the test will check if all the required calibration data exists. If it is not, an error message will be prompted to ask you to enter the data.
In the situation where you choose to run the VSWR and Calibration Factor with additional frequency points, the test setup verification in the said tests will only verify the factory predefined data points.
If the calibration data of the additional frequency points for the power splitter or standard power sensor are not available, linear interpolated calibration data will be generated and used for those points when calculating calibration factor and the associated uncertainty.
, where y is the calibration data and x is the frequency associated with the calibration data.
Table 1 lists the UUT factory predefined frequency points at which the calibration data is required for the external test equipment (ETEs) for each UUT model.
Table 2 lists the equipment that needs to be calibrated at the specific frequency points listed in Table 1.
Please have your ETEs calibrated at those frequency points and enter the calibration data in TME before you run any test.
| Frequency (GHz) | N8481A, N8481A Opt 200, 8481A, N8481B, N8481H |
N8482A*, N8482B, N8482H |
8482A* | N8485A | N8485A Opt 033 | 8485A, 8485D | 8487A, N8487A | N8488A | N8486AR | N8486AQ | E9304A* | E9304A Opt H18* |
| 0.000009 | X | X | ||||||||||
| 0.00003 | X | X | ||||||||||
| 0.00005 | X | X | ||||||||||
| 0.0001 |
X | X | X | X | ||||||||
| 0.0003 | X | X | X | X | ||||||||
| 0.0005 | X | X | X | X | ||||||||
| 0.001 | X | X | X | X | ||||||||
| 0.003 | X | X | X | X | ||||||||
| 0.005 | X | X | X | X | ||||||||
| 0.01 | X | X | X | X | X | X | X | X | ||||
| 0.02 | X | |||||||||||
| 0.03 | X | X | X | X | X | X | X | X | ||||
| 0.04 | X | |||||||||||
| 0.05 | X | X | X | X | X | X | X | X | X | X | ||
| 0.1 |
X | X | X | X | X | X | X | X | X | X | ||
| 0.3 | X | X | X | X | X | X | X | X | X | X | ||
| 0.5 | X | X | X | X | X | X | X | X | X | X | ||
| 0.8 | X | X | ||||||||||
| 1 | X | X | X | X | X | X | X | X | X | X | ||
| 1.2 | X | X | ||||||||||
| 1.5 | X | X | X | X | X | X | X | X | ||||
| 2 | X | X | X | X | X | X | X | X | X | X | ||
| 2.5 | X | X | ||||||||||
| 3 | X | X | X | X | X | X | X | X | X | X | ||
| 3.5 | X | |||||||||||
| 4 | X | X | X | X | X | X | X | X | X | X | ||
| 4.2 | X | X | ||||||||||
| 5 | X | X | X | X | X | X | X | X | X | |||
| 6 | X | X | X | X | X | X | X | X | X | |||
| 1 GHz step | X | X | X | X | X | X | X | |||||
| 12 |
X | X | X | X | X | X | X | |||||
| 12.4 |
X | X | X | X | X | X | ||||||
| 13 |
X | X | X | X | X | X | X | |||||
| 1 GHz step |
X | X | X | X | X | X | X | |||||
| 18 | X | X | X | X | X | X | X | |||||
| 1 GHz step |
X | X | X | X | X | |||||||
| 26 |
X | X | X | X | X | |||||||
| 26.5 |
X | X | X | X | X | |||||||
| 27 | X | X | X | X | ||||||||
| 1 GHz step | X | X | X | X | ||||||||
| 33 | X | X | X | X | X | |||||||
| 34 | X | X | X | X | ||||||||
| 34.5 | X | X | X | |||||||||
| 35 | X | X | X | X | ||||||||
| 1 GHz step | X | X | X | X | ||||||||
| 40 | X | X | X | X | ||||||||
| 1 GHz step | X | X | X | |||||||||
| 50 | X | X | X | |||||||||
| 1 GHz step | X | |||||||||||
| 70 | X |
* N8482A, 8482A, E9304A, and E9304A Opt H18 Opt Z2092B-208 VSWR test, the start frequency point is 10 MHz.
|
|
You can order the following options to calibrate the test equipment to meet the TME requirement on the test equipment's calibration data.
|
| Equipment type | Performance test | ||||||||||
| VSWR | Linearity | Calibration Factor | |||||||||
| N8481A/8481A /N8481B/N8481H |
N8481A Opt 200 | N8482A/8482A /N8482B/N8482H |
N8485A/8485A /8485D |
N8485A Opt 033 | N8487A /8487A |
N8488A | N8486AR /N8486AQ |
E9304A /E9304A Opt H18 |
|||
| StandardPowerSensor1 |
UUT models, N8481A, N8482A, N8485A, 8481A, 8482A, 8485A, 8487A, 50 MHz only | + | + | + Range 2 |
+ | + | + | + | + | ||
| StandardPowerSensor2 |
+ Range 1 |
||||||||||
| StandardPowerSensorExtendedFrequency1 | + | ||||||||||
| VerificationPowerSensor1 |
+ | + | + Range 2 |
+ | + | + | + | + | |||
| VerificationPowerSensor2 |
+ Range 1 |
||||||||||
| VerificationPowerSensorExtendedFrequency1 | + | ||||||||||
| BuriedPowerSensor1 |
+ | + | + Range 2 |
+ | + | + | + | + | |||
| BuriedPowerSensor2 |
+ Range 1 |
||||||||||
| BuriedPowerSensorExtendedFrequency1 | + | ||||||||||
| LinearityReferencePowerSensor | UUT models: 8485D, E9304A, E9304A Opt H18, N8487A, N8488A, N8481B, N8482B, N8481H, N8482H, N8486AQ, N8486AR, 50 MHz only |
||||||||||
| Splitter1 |
+ | + Range 2 |
+ | ||||||||
| Splitter2 |
+ Range 1 |
||||||||||
| PowerSplitter1 3.5 mm F | + | + | |||||||||
| PowerSplitter1 2.4 mm F | + | ||||||||||
| PowerSplitter1 1.85 mm F | + | ||||||||||
| PowerSplitter1 APC7 F | + | ||||||||||
| Network Analyzer 1-Port Cal Verification Device 1 | + All UUT models, except N8481A Opt 200 and N8485A Opt 033[*] |
||||||||||
| Network Analyzer 1-Port Cal Verification Device 2 | + N8481A Opt 200 and N8485A Opt 033 |
||||||||||
+Refer to Table 1 for the required frequency points.
Range 1: 100 kHz to 50 MHz
Range 2:
* If an E9340A power sensor is used, the frequency points 2.5 GHz, 3.5 GHz, and 4.2 GHz are not required.
To enter the Device (power splitter or power sensor) calibration data into TME, follow these steps if electronic copy of the calibration data is available:
Z2092B-208 is a predefined TME calibration option for the Z2092B-207 power sensor test system. The Z2092B-207 power sensor test system with Option Z2092B-208 has a network analyzer lower frequency limit of 10 MHz. If this option is selected during the order creation of an N8482A unit under test (UUT), a limited calibration will be performed on the UUT.
VSWR will only be measured from 10 MHz to 6 GHz. The determination of Calibration Factor assumes that the UUT meets its VSWR specifications for frequencies below 10 MHz. This results in higher Calibration Factor uncertainty for this limited calibration below 10 MHz.
The calibration data of the splitters and standard and verification power sensors is still required for the full frequency range of 100 kHz to 6 MHz. (See Table 1 for the required calibration data.)
TME supports two types of power sensor labels:
Power Sensor Calibration Data Label (N8481-84306) — the Keysight N8481-84306 power sensor label for the N8480 Series CFT sensor
|
|
There is no Calibration Data Label required for the E9304A, N8488A, and the N8480 Series Opt STD power sensors in this calibration application. |
The data on the sensor label will include the model number and serial number of the sensor as well as the calibration data (frequency, calibration factor, and rho) for the predefined frequencies.
To print or view the label, go to the Test Reports tab, select one of the label templates from the Report Template’s drop down list, then select the desired Calibration Factor test run. Finally click the Create Report button to view the label. You can either print the label directly from the TME report viewer or save the report to a pdf file then print it from a pdf viewer.
The TME report viewer will only use the default printer. If you would like to print the label from the report viewer, please set the default printer to the desired label printer before creating the label report in TME.
The driver for the Zebra printers can be downloaded from Zebra Technologies. The information of the discontinued printers can be found here.
To set the printing preferences, please select the Printers and Faxes submenu from the Start menu, then double-click on the printer. Select the Printing Preferences... from the Printer menu. Configure the printer settings through the Printing Preferences dialog box.
Please recalibrate the printer after changing the media or ribbon.
Please check the printer settings after changing the media.
The TLP 3842 printer prefers an approximately 1/8” gap between labels. The 08481-80115 label has an approximately 1” gap and was not supported for the TLP 3842.
The following printer settings were tested on Zebra 90 XiII and TLP 3842. Please set the Gap/Mark Height, Size, and Paper Format accordingly. You may also need to adjust the Speed, Darkness, and Tear Off Adjustment for your particular printer. For the other printer settings, please use the default values.
| TLP 3842 | Zebra 90 XiII | |
|
Gap/Mark Height |
0.12” |
NA |
|
Size |
1.5" × 3.5" (Width × Height) |
1.5" × 3.5" (Width × Height) |
|
Paper Format |
Rotate 180 |
No Rotate |
|
Speed |
1.5"/s |
2 |
|
Darkness |
15 (TLP 2844) |
15 |
|
Tear Off Adjustment |
N/A |
–0.08” |
| Media | Thermal Transfer Label with Gaps |
Thermal Transfer Web Sensing |
| Zebra 90 XiII | |
|
Gap/Mark Height |
NA |
|
Size |
3.5" × 5" (Width × Height) |
|
Paper Format |
Rotate 180 |
|
Speed |
2 |
|
Darkness |
15 |
|
Tear Off Adjustment |
–0.39” |
| Media | Thermal Transfer Web Sensing |