|
|
There are specific configuration requirements for a TME test station running the N7874A calibration software. Refer to the TME Test Station Configuration Requirements in the Getting Started topic. |
This section lists the test equipment needed to run performance tests. Models for each test equipment category are given in order of preference. Alternate models are also listed but should be considered a lower priority. All equipment is Keysight, Agilent, or Hewlett Packard unless otherwise specified. Refer to each individual test for specific setup configurations. The computer and all test equipment are connected to the device under test (DUT) using GPIB and PXI.
|
Test Equipment |
Recommended Model |
Alternate Model |
|
PNA network analyzer |
N5245B |
N5247B N5222A N5242A E8363C |
|
Power meter |
N1914A1 |
N1912A |
|
Power sensor
|
N8485A |
None
|
|
Frequency counter |
53230A Option 115 |
53131A |
|
Frequency reference2 |
Frequency counter internal |
House standard |
|
Dynamic accuracy test set |
U3020BD01 |
U3020A-D01 |
|
Compression test set |
U3070BK01 |
U3070A-K01 |
|
10 dB fixed attenuator
|
8493C Option 010 |
None |
|
Load, 50 Ω, 3.5 mm
|
909D Option 301 |
909D Option 040 |
|
Calibration kit, 3.5 mm |
85052B |
85052D |
|
ECal module, 3.5 mm |
N4691D3 Option M0F |
N4691-60004 |
|
PXIe chassis
|
M9018B |
M9018A |
|
Embedded controller4
|
M9037A |
|
|
Cables |
||
|
RF 3.5 mm (m) to 3.5 mm (f)
|
8121-2111 |
|
|
Adapters |
||
|
3.5 mm (f) to 3.5 mm (f) |
83059B |
1250-1749 |
|
3.5 mm (m) to 2.4 mm (m)
|
11904A |
|
|
3.5 mm (m) to Type-N (m) |
1250-1743 |
|
|
BNC (m) to Type-N (f) |
1250-1477 |
|
|
3.5 mm (m) to 3.5 mm (m)
|
83059A |
1250-1748 |
|
Use the following guidelines to ensure power sensors used by the N7800A application receive the correct calibration service:
Order Option 1A7 when ordering new power sensors that will be used as working standards in N7800A TME calibrations.
Order the Keysight Cal + Measurement Uncertainty + GB calibration service for power sensor recalibration.
When ordering periodic calibration for instruments used as lab standards in the N7800A software, we recommend using “Keysight calibration + uncertainties” for power sensors, and “Keysight calibration + uncertainties + guardbanding” for all other items (please visit Selecting the Right Calibration Services). The N7800A software incorporates the ISO GUM Uncertainty in point-to-point uncertainty calculations. The special “H-series” calibration options in this table provide lower measurement uncertainties through use of direct comparison to devices directly characterized by NPL or NIST (or another NMI). Please order Option H99 to get electronic data for easy import into the N7800A (avoids manual entry). The overall resulting N7800A measurement uncertainties then reflects these lower device uncertainties. The equipment requirements of each N7800A calibration application are summarized in the specials calibration matrix which can be found at the Recommended Lab Standards and Special Cal Options website.
The Keysight Option H99 is a special option for the Roseville Service Center [only] which provides electronic calibration data available as a .csv file in TME N7800A format for all power sensors used with the N7800A TME application. N7800A TME is SSU calibration software used across Keysight SSU and by many self-maintainers. H99 must be requested from the Roseville SSU upon re-calibration only of any previously purchased power sensor and not for new purchases of BID Power Sensors. This option may be ordered in addition to any other required or requested Std Lab Calibration option (must also be ordered in addition to H99). Option H99 is recommended but not required.
|
|
The following models are not supported by Option H99:
|