In this procedure, the instrument is turned ON, set to Internal Reference mode, and allowed to warm up for 30 minutes (except for CXA-m with Option PFR is 15 minutes). The frequency of the 10 MHz Reference is measured at the DUT's 10 MHz Out port using a frequency counter which is locked to a primary frequency standard. The measured value is compared to the allowable offset guideline and is included in the Performance Test printout.
|
Test Equipment |
Recommended Model Number1 |
|---|---|
|
Frequency counter |
53230A |
|
Frequency standard2 |
5071A |
|
Cable, BNC |
8120-2582 |
|
Cable, BNC (m) to SMB (f) |
8121-2063 |
|