Frequency Span Accuracy is a measure of the CXA-m's sweep linearity. The test is done in several spans to check all modes of the synthesizer circuitry.
The generator signal is placed at the first graticule in the span and the frequency is read. Then the generator signal is placed at the ninth graticule of the span and the frequency is measured. The frequency difference is compared to 0.80 * Span setting. Since the source is locked to the CXA-m reference, the source frequency error is zero.
|
Test Equipment |
Recommended Model Number1 |
|---|---|
|
Microwave signal generator #1 |
PSG models |
|
Cable, BNC (m) to SMB (f) |
8121-2063 |
|
Coaxial cable, 3.5 mm (m) to 3.5 mm (m) |
11500E |
|
Adapter, 3.5 mm (f) to 3.5 mm (f)
|
83059B |
|
Adapter, 2.4 mm (f) to 3.5 mm (f)
|
11901B |
|