Phase Noise Performance Test

This test verifies the analyzer noise sideband specification. The source can be either a Wenzel Ultra Low Noise source or a PSG. The Wenzel is the preferred solution.

The test requires that DANL at 1 GHz be characterized for the near noise corrections. If the DANL test has been run, the DANL test data will be used. If DANL has not been run, then the DANL will be characterized at 1 GHz.

Required Test Equipment

Test Equipment

Recommended Model Number1

Ultra low noise reference frequency source

Wenzel 500-13438 Rev D

Microwave signal generator #1
(for alternate setup)

PSG models
(see main equipment list)

Attenuator, 10 dB fixed

  • Only required when using the Wenzel setup

8493C Option 010

Termination, 3.5 mm (m)

909D

Cable, BNC (m) to SMB (f)

  • Only required when using the PSG setup

8121-2063

Coaxial cable, 3.5 mm (m) to 3.5 mm (m)

11500E

Adapter, 3.5 mm (f) to 3.5 mm (f)

  • Only required when using a 3.5 mm PSG

83059B

Adapter, 2.4 mm (f) to 3.5 mm (f)

  • Only required when using a 2.4 mm PSG

11901B

  1. Refer to the main equipment list for a list of alternative models (if available).

Connection Setups

DANL Setup

Wenzel Source Rear Panel Switch Settings

Phase Noise Test Setup Using a Wenzel Source

Phase Noise Test Setup Using a PSG Source