Spurious Responses Performance Test

This test verifies that the analyzer meets its specification for input related spurious responses. In this test, the source is connected to the RF Input and set for the spur frequency. The source amplitude is measured using a power meter. The source frequency is then moved to the frequency location that will create the spur at the analyzer center frequency. The amplitude of the source is kept consistent by using the power meter. The analyzer then measures the spurious response at the spur frequency.

Required Test Equipment

Test Equipment

Recommended Model Number1

Microwave signal generator #1

PSG models
(see main equipment list)

Power meter

N1914A

Microwave power sensor

N8485A CFT

Power splitter

11667B

Cable, BNC (m) to SMB (f)

8121-2063

Cable, Coaxial, 3.5 mm (m) to 3.5 mm (m)

11500E

Adapter, 3.5 mm (m) to 3.5 mm (m)2

83059A

Adapter, 3.5 mm (f) to 3.5 mm (f)

  • For 3.5 mm source

83059B

Adapter, 2.4 mm (f) to 3.5 mm (f)

  • For 2.4 mm source

11901B

Adapter, 3.5 mm (f) to Type-N (m)

  • For the 8485A power sensor

08485-60005

  1. Refer to the main equipment list for a list of alternative models (if available).
  2. The 3.5 mm (m) to 3.5 mm (m) adapter between the power splitter and the DUT is critical in this test. Proper connector care and torqueing practices must be followed in order to insure optimal performance.

Connection Setups

Power Meter Calibration

 

Spurious Responses Test Setup