Keysight 89600 VSA .NET API
AnalogDemodAMUnitType Enumeration
See Also 
Agilent.SA.Vsa.AnalogDemod.Interfaces Assembly > Agilent.SA.Vsa.AnalogDemod Namespace : AnalogDemodAMUnitType Enumeration


Glossary Item Box

Specifies the AM modulation index units.

Syntax

Visual Basic (Declaration) 
Public Enum AnalogDemodAMUnitType 
   Inherits System.Enum
C# 
public enum AnalogDemodAMUnitType : System.Enum 
C++/CLI 
public enum class AnalogDemodAMUnitType : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
AMSpecifies AM modulation index in numeric units.
PercentSpecifies AM modulation index in percent units.
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also