| Class | Description | |
|---|---|---|
![]() | AnalogDemodChannel | The AnalogDemodChannel object represents the demodulation settings for one input channel. |
![]() | AnalogDemodChannelCollection | This collection contains the set of AnalogDemodChannel objects representing the demodulation settings for each logical input channel. |
![]() | MeasurementExtension | The AnalogDemod.MeasurementExtension object contains properties and members to control the Analog Demodulation measurement features. |
| Enumeration | Description | |
|---|---|---|
![]() | AnalogDemodAMUnitType | Specifies the AM modulation index units. |
![]() | AnalogDemodType | Specifies the type of analog demodulation to perform for the input channel. |