Keysight 89600 VSA .NET API
MeasurementExtension Class
Members  See Also 
Agilent.SA.Vsa.AnalogDemod.Interfaces Assembly > Agilent.SA.Vsa.AnalogDemod Namespace : MeasurementExtension Class


Glossary Item Box

The AnalogDemod.MeasurementExtension object contains properties and members to control the Analog Demodulation measurement features.

Object Model

MeasurementExtension ClassMeasurementExtension ClassMeasurementExtension ClassMeasurementExtension ClassAnalogDemodChannelCollection ClassAnalogDemodChannelCollection ClassAnalogDemodChannel ClassAnalogDemodChannelCollection ClassAnalogDemodChannel Class

Syntax

Visual Basic (Declaration) 
Public MustInherit Class MeasurementExtension 
   Inherits Agilent.SA.Vsa.MeasurementExtension
   Implements Agilent.SA.Vsa.IMeasurementExtensionAgilent.SA.Vsa.IPropertyInfoAgilent.SA.Vsa.IPropertyInfo2Agilent.SA.Vsa.IRemoteNotifyPropertyChangedAgilent.SA.Vsa.IRemoteNotifyPropertyInfoChanged, Agilent.SA.VsaInternal.IMeasurementBase, Agilent.SA.VsaInternal.IMeasurementBase2, Agilent.SA.VsaInternal.IMeasurementBase3, Agilent.SA.VsaInternal.IMeasurementBase4, Agilent.SA.VsaInternal.IMeasurementBase5, Agilent.SA.VsaInternal.IObjectModel, Agilent.SA.VsaInternal.IObjectModel2, Agilent.SA.VsaInternal.IObjectModel3 
C# 
public abstract class MeasurementExtension : Agilent.SA.Vsa.MeasurementExtension, Agilent.SA.Vsa.IMeasurementExtensionAgilent.SA.Vsa.IPropertyInfoAgilent.SA.Vsa.IPropertyInfo2Agilent.SA.Vsa.IRemoteNotifyPropertyChangedAgilent.SA.Vsa.IRemoteNotifyPropertyInfoChanged, Agilent.SA.VsaInternal.IMeasurementBase, Agilent.SA.VsaInternal.IMeasurementBase2, Agilent.SA.VsaInternal.IMeasurementBase3, Agilent.SA.VsaInternal.IMeasurementBase4, Agilent.SA.VsaInternal.IMeasurementBase5, Agilent.SA.VsaInternal.IObjectModel, Agilent.SA.VsaInternal.IObjectModel2, Agilent.SA.VsaInternal.IObjectModel3  
C++/CLI 
public ref class MeasurementExtension abstract : public Agilent.SA.Vsa.MeasurementExtension, Agilent.SA.Vsa.IMeasurementExtensionAgilent.SA.Vsa.IPropertyInfoAgilent.SA.Vsa.IPropertyInfo2Agilent.SA.Vsa.IRemoteNotifyPropertyChangedAgilent.SA.Vsa.IRemoteNotifyPropertyInfoChanged, Agilent.SA.VsaInternal.IMeasurementBase, Agilent.SA.VsaInternal.IMeasurementBase2, Agilent.SA.VsaInternal.IMeasurementBase3, Agilent.SA.VsaInternal.IMeasurementBase4, Agilent.SA.VsaInternal.IMeasurementBase5, Agilent.SA.VsaInternal.IObjectModel, Agilent.SA.VsaInternal.IObjectModel2, Agilent.SA.VsaInternal.IObjectModel3  

Remarks

You can select independent demodulation settings for each input channel, but only one demodulation type on each channel.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also