Visual Basic (Declaration) | |
---|---|
Public Enum ChannelResponseScaling Inherits System.Enum |
C# | |
---|---|
public enum ChannelResponseScaling : System.Enum |
C++/CLI | |
---|---|
public enum class ChannelResponseScaling : public System.Enum |
Member | Description | Minimum SW Version‡ |
---|---|---|
Absolute | Peak of impulse response will match band power markers on Spectrum trace (when only one path). | — |
Relative | Peak of impulse response will read 0 dB when only one path. | — |
‡ This is the minimum 89600 VSA software version level needed to use this enum member. |
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)