Class | Description | |
---|---|---|
![]() | MeasurementExtension | The MeasurementExtension class contains properties and control the Channel Sounding measurement. |
Enumeration | Description | |
---|---|---|
![]() | ChannelResponseScaling | Normalization mode for impulse response. |
![]() | FilterType | Filter type to apply to the signal. |
![]() | FrequencyCompensationSource | Source of frequency correction applied to signal. |
![]() | RmsDelaySpreadPathIncludeMode | Specifies which impulse response points to include when computing RMS Delay Spread and Average Delay. |
![]() | RmsDelaySpreadThresholdReference | Specifies the reference for the MeasurementExtension.RmsDelaySpreadThresholdOffset. |
![]() | SequenceLength | Base sequence length of channel sounding sequence. |
![]() | T0Location | Specifies the time t=0 location in the impulse response. |