Keysight Pathwave 89600 VSA .NET API
FrequencyCompensationSource Enumeration
See Also 
Agilent.SA.Vsa.ChannelSounding.Interfaces Assembly > Agilent.SA.Vsa.ChannelSounding Namespace : FrequencyCompensationSource Enumeration


Glossary Item Box

Source of frequency correction applied to signal.

Syntax

Visual Basic (Declaration) 
Public Enum FrequencyCompensationSource 
   Inherits System.Enum
C# 
public enum FrequencyCompensationSource : System.Enum 
C++/CLI 
public enum class FrequencyCompensationSource : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
AllChannelAverageErrorCorrect each channel by the average of all channels' frequency error estimates.
ChannelErrorCorrect each channel by its own frequency error estimate.
ReferenceChannelErrorCorrect each channel by the reference channel's frequency error estimate.
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also