Visual Basic (Declaration) | |
---|---|
Public Overridable Property ShowExtraImpulseResponseWidth As Boolean |
C# | |
---|---|
public virtual bool ShowExtraImpulseResponseWidth {get; set;} |
The valid portion of the impulse response is 2x the sequence length. Enabling this feature is useful for troubleshooting to see if the choice of SequenceLength is long enough for the delay spread of the channel.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)