Keysight 89600 VSA .NET API
ConstellationStateCollection Class
Members  See Also 
Agilent.SA.Vsa.CustomIQ.Interfaces Assembly > Agilent.SA.Vsa.CustomIQ Namespace : ConstellationStateCollection Class


Glossary Item Box

The ConstellationStateCollection class contains a collection of constellation state objects.

Object Model

ConstellationStateCollection ClassConstellationState ClassConstellationState Class

Syntax

Visual Basic (Declaration) 
Public MustInherit Class ConstellationStateCollection 
   Inherits Agilent.SA.Vsa.RemotableCollection(Of ConstellationState)
   Implements Agilent.SA.Vsa.ICollectionBase, Agilent.SA.Vsa.ICollectionBase(Of ConstellationState), Agilent.SA.Vsa.IPropertyInfo, Agilent.SA.Vsa.IPropertyInfo2, Agilent.SA.Vsa.IRemoteNotifyCollectionChanged, Agilent.SA.Vsa.IRemoteNotifyPropertyChanged, Agilent.SA.Vsa.IRemoteNotifyPropertyInfoChanged, Agilent.SA.VsaInternal.IObjectModel, Agilent.SA.VsaInternal.IObjectModel2, Agilent.SA.VsaInternal.IObjectModel3 

Remarks

The collection of constellation states (ConstellationState) fundamentally defines a constellation for use in Custom IQ modulation analysis.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 18.00

See Also