| Class | Description | |
|---|---|---|
![]() | Constellation | The Constellation class represents the definition of a constellation for use in Custom IQ modulation analysis. |
![]() | ConstellationState | This class is for setting parameters for individual states within a constellation defined for use in Custom IQ modulation analysis. |
![]() | ConstellationStateCollection | The ConstellationStateCollection class contains a collection of constellation state objects. |
![]() | MeasurementExtension | Measurement extension for CustomIQ |
![]() | QuickSetup | The CustomIQ.QuickSetup class contains properties and methods related to loading a user-defined measurement setup into a CustomIQ measurement extension. |
![]() | QuickSetupCollection | The CustomIQ.QuickSetupCollection class provides access to the CustomIQ.QuickSetup objects available to a CustomIQ measurement extension. |
| Structure | Description | |
|---|---|---|
![]() | ConstellationStateDescription | A simple constellation state struct that only has Real, Imaginary, and Symbol fields compared to ConstellationState. This is used when recalling a large number of constellation locations from a file that has Real, Imaginary, and Symbol fields like for a file generated by N7608B Signal Studio for Custom Modulation. |
| Enumeration | Description | |
|---|---|---|
![]() | ConstellationStyle | Presets for use as a starting point in creating a constellation definition. |
![]() | ConstellationSymbolMapSource | Source location from which to derive the constellation symbol map. |
![]() | EqualizerMode | Specifies the mode of the digital-demodulation adaptive equalizer. |
![]() | EqualizerType | Disables adaptive equalizer or specifies the type of the adaptive equalizer if it is enabled. |
![]() | FrequencyEstimationMode | Specifies the mode of the digital demodulation frequency estimation |
![]() | MeasurementFilter | Specifies the type of digital demodulation measurement filter to apply. |
![]() | NormalizationReference | Reference used for normalization of IQ results and EVM. |
![]() | PatternSearchSyncCriteria | Specifies the pattern search synchronization criteria used to determine a valid pattern detection. |
![]() | ReferenceFilter | Specifies the type of digital demodulation reference filter to apply. |