Keysight 89600 VSA .NET API
ConstellationSymbolMapSource Enumeration
See Also 
Agilent.SA.Vsa.CustomIQ.Interfaces Assembly > Agilent.SA.Vsa.CustomIQ Namespace : ConstellationSymbolMapSource Enumeration


Glossary Item Box

Source location from which to derive the constellation symbol map.

Syntax

Visual Basic (Declaration) 
Public Enum ConstellationSymbolMapSource 
   Inherits System.Enum
C# 
public enum ConstellationSymbolMapSource : System.Enum 
C++/CLI 
public enum class ConstellationSymbolMapSource : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
StateIndexesSymbol value for each ConstellationState always uses the ConstellationState.Index value.—
UserDefinedSymbolsSymbol value for each ConstellationState always uses the ConstellationState.Symbol value.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 18.00

See Also