Keysight 89600 VSA .NET API
EqualizerType Enumeration
See Also 
Agilent.SA.Vsa.CustomIQ.Interfaces Assembly > Agilent.SA.Vsa.CustomIQ Namespace : EqualizerType Enumeration


Glossary Item Box

Disables adaptive equalizer or specifies the type of the adaptive equalizer if it is enabled.

Syntax

Visual Basic (Declaration) 
Public Enum EqualizerType 
   Inherits System.Enum
C# 
public enum EqualizerType : System.Enum 
C++/CLI 
public enum class EqualizerType : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
MinimizeErrorVectorThe second type of equalizer, which minimizes error vector, is enabled.—
MinimizeEvmThe first type of equalizer, which minimizes EVM, is enabled.—
NoneEqualizer is disabled.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 25.00

See Also