| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property EqualizerConvergence As Double | |
| C# | |
|---|---|
public abstract double EqualizerConvergence {get; set;} | |
Controls the rate of convergence of the adaptive equalizer of the digital demodulation measurement. Convergence determines how quickly the equalization filter coefficients converge to the estimated Values for each measurement. Larger values converge faster. This provides a trade-off in the number of measurements required for convergence of the equalization filter taps, and the stability of those taps. This property is only useful if the adaptive equalizer is on (IsEqualized). Default Value: 1e-07. For more, see Digital Demodulation "Convergence (equalization)" topic in the VSA Application help.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 18.00