| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property EqualizerFilterLength As Integer | |
| C# | |
|---|---|
public abstract int EqualizerFilterLength {get; set;} | |
Specifies the length of the adaptive equalization filter of the digital demodulation measurement. The value is specified as an odd whole number of symbols. This property is only applied if the adaptive equalizer is enabled (IsEqualized). For more information, see the Digital Demodulation "Using the Equalization Filter" topic in the VSA Application help.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 18.00