| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property IsPatternSearchEnabled As Boolean | |
| C# | |
|---|---|
public abstract bool IsPatternSearchEnabled {get; set;} | |
Determine whether constellation sync search is enabled for the digital demodulation measurement. When true, SearchPattern determines the pattern to search for in the input data, and PatternSearchOffset determines where in the demodulated symbols the pattern should be located. The search process consists of demodulating the data at the different possible ideal constellation phase offsets, and aligning the symbols with the data pattern. If the data pattern cannot be found, a trace indicator of "SYNC NOT FOUND" is displayed.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 18.00