Keysight 89600 VSA .NET API
ResultLength Property
See Also 
Agilent.SA.Vsa.CustomIQ.Interfaces Assembly > Agilent.SA.Vsa.CustomIQ Namespace > MeasurementExtension Class : ResultLength Property


Glossary Item Box

Gets or sets the demodulation measurement result length (in symbols).

Syntax

Visual Basic (Declaration) 
Public MustOverride Property ResultLength As Integer
C# 
public abstract int ResultLength {get; set;}
C++/CLI 
public:
abstract property int ResultLength {
   int get();
   void set (    int value);
}

Remarks

This is used to determine the number of symbols to demodulate.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 18.00

See Also