Keysight 89600 VSA .NET API
CarrierAggregation Class
Members  See Also 
Agilent.SA.Vsa.CustomOfdm.Interfaces Assembly > Agilent.SA.Vsa.CustomOfdm Namespace : CarrierAggregation Class


Glossary Item Box

Settings for Custom OFDM Carrier Aggregation, where multiple component carriers are measured from a single (synchronous) or per-carrier (sequential) acquisition.

Object Model

CarrierAggregation ClassComponentCarrierCollection ClassComponentCarrier ClassFbmcSettings ClassFrameCreationUtility ClassMulticarrierFilter ClassNomaSettings ClassScmaSettings ClassComponentCarrier ClassFbmcSettings ClassFrameCreationUtility ClassMulticarrierFilter ClassNomaSettings ClassScmaSettings Class

Syntax

Visual Basic (Declaration) 
Public MustInherit Class CarrierAggregation 
   Inherits Agilent.SA.Vsa.RemotableObject
   Implements Agilent.SA.Vsa.IPropertyInfo, Agilent.SA.Vsa.IPropertyInfo2, Agilent.SA.Vsa.IRemoteNotifyPropertyChanged, Agilent.SA.Vsa.IRemoteNotifyPropertyInfoChanged, Agilent.SA.VsaInternal.IObjectModel, Agilent.SA.VsaInternal.IObjectModel2, Agilent.SA.VsaInternal.IObjectModel3 
C# 
public abstract class CarrierAggregation : Agilent.SA.Vsa.RemotableObject, Agilent.SA.Vsa.IPropertyInfo, Agilent.SA.Vsa.IPropertyInfo2, Agilent.SA.Vsa.IRemoteNotifyPropertyChanged, Agilent.SA.Vsa.IRemoteNotifyPropertyInfoChanged, Agilent.SA.VsaInternal.IObjectModel, Agilent.SA.VsaInternal.IObjectModel2, Agilent.SA.VsaInternal.IObjectModel3  
C++/CLI 
public ref class CarrierAggregation abstract : public Agilent.SA.Vsa.RemotableObject, Agilent.SA.Vsa.IPropertyInfo, Agilent.SA.Vsa.IPropertyInfo2, Agilent.SA.Vsa.IRemoteNotifyPropertyChanged, Agilent.SA.Vsa.IRemoteNotifyPropertyInfoChanged, Agilent.SA.VsaInternal.IObjectModel, Agilent.SA.VsaInternal.IObjectModel2, Agilent.SA.VsaInternal.IObjectModel3  

Remarks

To configure multiple component carriers remotely, set each carrier through ComponentCarriers.

Carrier indexes are zero-based and match the carrier names shown in the user interface: ComponentCarriers[0] is CC0, ComponentCarriers[1] is CC1, and so on.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 31.00

See Also