Keysight 89600 VSA .NET API
RemotableObject Class
Members  See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : RemotableObject Class


Glossary Item Box

Note that this class is intentionally split into two parts - this one, which is .NET 4.0 dependent and contains implementation used by 89600 VSA, and the other part which is merely a place-holder and is intended to be targeted to either a .NET 3.5 or .NET 4.0 platform. Provides the common base class for all classes defining the public API for the Keysight 89600 VSA software.

Syntax

Visual Basic (Declaration) 
Public MustInherit Class RemotableObject 
   Inherits System.MarshalByRefObject
   Implements IPropertyInfo, IPropertyInfo2, IRemoteNotifyPropertyChanged, IRemoteNotifyPropertyInfoChanged 

Remarks

Inheritance from IRemoteNotifyPropertyInfoChanged added in version 14.00.

Inheritance from IPropertyInfo2 added in version 23.20.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also