Keysight 89600 VSA .NET API
Remove Method
See Also 
Agilent.SA.Vsa.CustomOfdm.Interfaces Assembly > Agilent.SA.Vsa.CustomOfdm Namespace > ComponentCarrierCollection Class : Remove Method


item
ComponentCarrier to remove.

Glossary Item Box

Removes the indicated ComponentCarrier from the collection.

Syntax

Visual Basic (Declaration) 
Public MustOverride Function Remove( _
   ByVal item As ComponentCarrier _
) As Boolean
C# 
public abstract bool Remove( 
   ComponentCarrier item
)
C++/CLI 
public:
abstract bool Remove( 
   ComponentCarrier^ item
) 

Parameters

item
ComponentCarrier to remove.

Return Value

True if removed; otherwise false.

Remarks

The minimum number of ComponentCarrier items is 1.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also