Keysight 89600 VSA .NET API
ComponentCarrier Class
Members  See Also 
Agilent.SA.Vsa.CustomOfdm.Interfaces Assembly > Agilent.SA.Vsa.CustomOfdm Namespace : ComponentCarrier Class


Glossary Item Box

Settings for a single component carrier in a Custom OFDM Carrier Aggregation configuration.

Object Model

ComponentCarrier ClassFbmcSettings ClassFrameCreationUtility ClassFrameDefinition ClassAllocationCollection ClassFramePartCollection ClassMulticarrierFilter ClassNomaSettings ClassScmaSettings Class

Syntax

Visual Basic (Declaration) 
Public MustInherit Class ComponentCarrier 
   Inherits Agilent.SA.Vsa.RemotableObject
   Implements Agilent.SA.Vsa.IPropertyInfo, Agilent.SA.Vsa.IPropertyInfo2, Agilent.SA.Vsa.IRemoteNotifyPropertyChanged, Agilent.SA.Vsa.IRemoteNotifyPropertyInfoChanged, Agilent.SA.VsaInternal.IObjectModel, Agilent.SA.VsaInternal.IObjectModel2, Agilent.SA.VsaInternal.IObjectModel3 
C# 
public abstract class ComponentCarrier : Agilent.SA.Vsa.RemotableObject, Agilent.SA.Vsa.IPropertyInfo, Agilent.SA.Vsa.IPropertyInfo2, Agilent.SA.Vsa.IRemoteNotifyPropertyChanged, Agilent.SA.Vsa.IRemoteNotifyPropertyInfoChanged, Agilent.SA.VsaInternal.IObjectModel, Agilent.SA.VsaInternal.IObjectModel2, Agilent.SA.VsaInternal.IObjectModel3  
C++/CLI 
public ref class ComponentCarrier abstract : public Agilent.SA.Vsa.RemotableObject, Agilent.SA.Vsa.IPropertyInfo, Agilent.SA.Vsa.IPropertyInfo2, Agilent.SA.Vsa.IRemoteNotifyPropertyChanged, Agilent.SA.Vsa.IRemoteNotifyPropertyInfoChanged, Agilent.SA.VsaInternal.IObjectModel, Agilent.SA.VsaInternal.IObjectModel2, Agilent.SA.VsaInternal.IObjectModel3  

Remarks

Each component carrier is an independent single-carrier Custom OFDM signal tuned to its own center frequency. Carriers typically share the same OFDM frame structure and differ only in their preamble/pilot values. When All is selected in the Component Carrier diagram, the same edit can apply to every carrier.

Remote clients cannot select All; configure each carrier through ComponentCarriers. See CarrierAggregation for index mapping.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 31.00

See Also