Creates a custom modulation state using a pair of real/imaginary values and a symbol value.
Syntax
Parameters
- real
- The real value describing this custom modulation.
- imaginary
- The imaginary value describing this custom modulation.
- symbol
- The symbol value describing this custom modulation.
Return Value
A custom modulation state representing the input parameters.
Remarks
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
See Also