| Visual Basic (Declaration) | |
|---|---|
Public Overridable Function GetCyclicSuffixPerSymbol() As Single() | |
| C# | |
|---|---|
public virtual float[] GetCyclicSuffixPerSymbol() | |
| C++/CLI | |
|---|---|
public: virtual array<float>^ GetCyclicSuffixPerSymbol(); | |
Return Value
The cyclic suffix guard interval of each OFDM symbol.If the size of the array is less than the result length, processing loops back to the symbol number specified by GuardIntervalRepeatIndex.
When the ModulationScheme is set to ModulationScheme.Fbmc, this property is ignored, because FBMC does not use a cyclic suffix.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 29.00