Keysight 89600 VSA .NET API
FrameDefinition Class Members
See Also  Properties  Methods  Events
Agilent.SA.Vsa.CustomOfdm.Interfaces Assembly > Agilent.SA.Vsa.CustomOfdm Namespace : FrameDefinition Class

Glossary Item Box

The following tables list the members exposed by FrameDefinition.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyAllocationsGets a reference to the collection of Allocation settings.  —
Public PropertyCrossCorrelatedEvmEnabledGets or sets a value indicating whether to enable cross-correlated EVM.  29.00
Public PropertyFftLengthGets or sets the OFDM FFT length.  —
Public PropertyGuardIntervalRepeatIndexGets or sets how to loop back if the end of the specified cyclic prefix/suffix guard interval property arrays is reached.  —
Public PropertyHalfSubcarrierShiftEnabledGets or sets a value indicating whether to enable the half subcarrier shift.  —
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertyIsPilotDefinedInTimeDomainGets or sets a value indicating whether Pilot is defined in time domain.  29.00
Public PropertyIsSignalBurstedGets or sets a value indicating whether to enable the signal is bursted property.  29.00
Public PropertyModulationSchemeGets or sets a value indicating the modulation scheme.  29.00
Public PropertyMultipleAccessSchemeGets or sets a value indicating the multiple access scheme.  29.00
Public PropertyNumberOfLowerGuardSubcarriersGets or sets the number guard subcarriers below the used subcarriers.  —
Public PropertyNumberOfUpperGuardSubcarriersGets or sets the number guard subcarriers above the used subcarriers.  —
Public PropertyOfdmSystemSampleFrequencyGets or sets the OFDM system sample frequency (Hz).  —
Public PropertyPartsGets a reference to the collection of FramePart settings.  —
Public PropertyResourceMapLengthInSymbolsGets or sets the length of the resource map in number of symbols.  —
Public PropertySymbolStartIndexForResourceMapRepeatGets or sets how to loop back if the end of ResourceMap is reached.  —
Public PropertyTimeGapsRepeatIndexGets or sets how to loop back if the end of SetTimeGapPerSymbol is reached.  29.00
Public PropertyTransmitterAntennasGets or sets the total number of transmitter antennas used for the measurement.  29.00
Public PropertyTransmitterWindowBetaGets or sets the time-domain windowing between symbols.  29.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetCyclicSuffixPerSymbolGets the cyclic suffix guard interval of each OFDM symbol, as a fraction of the IFFT time length.  29.00
Public MethodGetGuardIntervalPerSymbolGets the cyclic prefix guard interval of each OFDM symbol, as a fraction of the IFFT time length.  —
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodGetTimeGapPerSymbolGets the time gap before each OFDM symbol, defined in samples at the OFDM system sample frequency.  29.00
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodSetCyclicSuffixPerSymbolSets the cyclic suffix guard interval of each OFDM symbol, as a fraction of the IFFT time length.  29.00
Public MethodSetGuardIntervalPerSymbolSets the cyclic prefix guard interval of each OFDM symbol, as a fraction of the IFFT time length.  —
Public MethodSetTimeGapPerSymbolSets the time gap before each OFDM symbol, defined in samples at the OFDM system sample frequency.  29.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also