| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Function GetGuardIntervalPerSymbol() As Single() | |
| C# | |
|---|---|
public abstract float[] GetGuardIntervalPerSymbol() | |
| C++/CLI | |
|---|---|
public: abstract array<float>^ GetGuardIntervalPerSymbol(); | |
Return Value
The cyclic prefix guard interval of each OFDM symbol.If the size of the array is less than the result length, processing loops back to the symbol number specified by GuardIntervalRepeatIndex.
When the ModulationScheme is set to ModulationScheme.Fbmc, this property is ignored, because FBMC does not use a cyclic prefix.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)