Gets or sets a value indicating whether to enable the half subcarrier shift.
Syntax
| Visual Basic (Declaration) | |
|---|
Public MustOverride Property HalfSubcarrierShiftEnabled As Boolean |
| C# | |
|---|
public abstract bool HalfSubcarrierShiftEnabled {get; set;} |
| C++/CLI | |
|---|
public:
abstract property bool HalfSubcarrierShiftEnabled {
bool get();
void set ( bool value);
} |
Property Value
The default value is false.
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
See Also