Keysight 89600 VSA .NET API
OfdmSystemSampleFrequency Property
See Also 
Agilent.SA.Vsa.CustomOfdm.Interfaces Assembly > Agilent.SA.Vsa.CustomOfdm Namespace > FrameDefinition Class : OfdmSystemSampleFrequency Property


Glossary Item Box

Gets or sets the OFDM system sample frequency (Hz).

Syntax

Visual Basic (Declaration) 
Public MustOverride Property OfdmSystemSampleFrequency As Double
C# 
public abstract double OfdmSystemSampleFrequency {get; set;}
C++/CLI 
public:
abstract property double OfdmSystemSampleFrequency {
   double get();
   void set (    double value);
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also