| Visual Basic (Declaration) | |
|---|---|
Public Overridable Property TransmitterAntennas As Integer | |
| C# | |
|---|---|
public virtual int TransmitterAntennas {get; set;} | |
Property Value
The value is limited to the number of Agilent.SA.Vsa.Input.MeasurementChannels defined in the Input configuration. When MeasurementExtension.CrossCorrelatedEvmEnabled = true, the maximum limit is half the number of Agilent.SA.Vsa.Input.MeasurementChannels.When total number of transmitter antennas is greater than one, the MIMO Configuration properties within FramePart and Allocation are enabled for use.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 29.00