Returns the type for instances this measurement extension. Some tools are unable to use the generic methods provided on
Agilent.SA.Vsa.Measurement class, so this is provided as an alternative.
Syntax
| Visual Basic (Declaration) | |
|---|
Public Shared Function ExtensionType() As Type |
| C# | |
|---|
public static Type ExtensionType() |
| C++/CLI | |
|---|
public:
static Type^ ExtensionType(); |
Return Value
A
System.Type object for the
MeasurementExtension type.
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
See Also